<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: NFC PN532</title>
    <link>https://community.nxp.com/t5/NFC/NFC-PN532/m-p/1757738#M10979</link>
    <description>&lt;P&gt;Hello Brian,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;What "&lt;SPAN&gt;wireless power" are you using? It is Qi Charging? At which frequency?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Typically there is no need to add any High pass filter since the Qi charger works at a different frequency than NFC. Also, these two systems should not work at the same time -&amp;gt; First NFC (typically check if there is some card in the proximity), If no, then WPT starts.&lt;/P&gt;
&lt;P&gt;In case you see some interference from the WPT source, you have to check the PN532 Rx Gain and if needed decrease it.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Tomas_Parizek_0-1700063371012.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/250010i8A5836883EED7821/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Tomas_Parizek_0-1700063371012.png" alt="Tomas_Parizek_0-1700063371012.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Tomas_Parizek_0-1700063371012.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 15 Nov 2023 15:49:43 GMT</pubDate>
    <dc:creator>Tomas_Parizek</dc:creator>
    <dc:date>2023-11-15T15:49:43Z</dc:date>
    <item>
      <title>NFC PN532</title>
      <link>https://community.nxp.com/t5/NFC/NFC-PN532/m-p/1755698#M10964</link>
      <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;I am Brian and would like help some guidelines on coexist between wireless power and NFC.&lt;/P&gt;&lt;P&gt;I have observed via oscilloscope and when WPT is running the NFC RX or TX or a snooping probe can see a strong modulation on the 13.56MHz OOK signal.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I am planning to add a high pass filter, should it injected to which location?&lt;/P&gt;&lt;P&gt;1) Before damping resistor after antenna coil&lt;/P&gt;&lt;P&gt;2) between matching and EMC filter&lt;/P&gt;&lt;P&gt;3) RX path (no idea which is the best point)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Fri, 10 Nov 2023 15:58:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-PN532/m-p/1755698#M10964</guid>
      <dc:creator>briansune</dc:creator>
      <dc:date>2023-11-10T15:58:12Z</dc:date>
    </item>
    <item>
      <title>Re: NFC PN532</title>
      <link>https://community.nxp.com/t5/NFC/NFC-PN532/m-p/1757738#M10979</link>
      <description>&lt;P&gt;Hello Brian,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;What "&lt;SPAN&gt;wireless power" are you using? It is Qi Charging? At which frequency?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Typically there is no need to add any High pass filter since the Qi charger works at a different frequency than NFC. Also, these two systems should not work at the same time -&amp;gt; First NFC (typically check if there is some card in the proximity), If no, then WPT starts.&lt;/P&gt;
&lt;P&gt;In case you see some interference from the WPT source, you have to check the PN532 Rx Gain and if needed decrease it.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Tomas_Parizek_0-1700063371012.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/250010i8A5836883EED7821/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Tomas_Parizek_0-1700063371012.png" alt="Tomas_Parizek_0-1700063371012.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Tomas_Parizek_0-1700063371012.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Nov 2023 15:49:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-PN532/m-p/1757738#M10979</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2023-11-15T15:49:43Z</dc:date>
    </item>
  </channel>
</rss>