<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 Re: Library for PN5180 with Raspberry Pi 4</title>
    <link>https://community.nxp.com/t5/NFC/Library-for-PN5180-with-Raspberry-Pi-4/m-p/1752917#M10951</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/369"&gt;@danielchen&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;which libs should we download, because the contents of the SW352236 folder do not work on raspbian. Lots of inclusion is missing. Can you directly provide a link to a C++ header to use the PN5180-nfc reader. Do you have an example without a GUI?&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;</description>
    <pubDate>Mon, 06 Nov 2023 15:46:10 GMT</pubDate>
    <dc:creator>fy</dc:creator>
    <dc:date>2023-11-06T15:46:10Z</dc:date>
    <item>
      <title>Library for PN5180 with Raspberry Pi 4</title>
      <link>https://community.nxp.com/t5/NFC/Library-for-PN5180-with-Raspberry-Pi-4/m-p/1374622#M9008</link>
      <description>&lt;P&gt;Hey,&lt;/P&gt;&lt;P&gt;I bought a RC522 for a project with a Raspberry Pi 4 but the RC522 has a short range. I need a range of at least 10 cm. So, I bought the PN5180, but now I can't find any working library. I want to use Python for this project, but a C++ or any other programming language library would also be fine. Is there any library available?&lt;/P&gt;&lt;P&gt;Here is the Hardware I want to use: Raspberry Pi 4 to control the reader, NFC Tag (NFC-Chip: NXP NTAG213, NFC-standard: ISO/IEC 14443-A, NFC Forum: Type 2), PN5180&lt;/P&gt;&lt;P&gt;Note: I want to read the UID and don't need to write to the chips.&lt;/P&gt;&lt;P&gt;Thanks, Konrad&lt;/P&gt;</description>
      <pubDate>Sat, 20 Nov 2021 20:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Library-for-PN5180-with-Raspberry-Pi-4/m-p/1374622#M9008</guid>
      <dc:creator>Konrad007</dc:creator>
      <dc:date>2021-11-20T20:26:48Z</dc:date>
    </item>
    <item>
      <title>Re: Library for PN5180 with Raspberry Pi 4</title>
      <link>https://community.nxp.com/t5/NFC/Library-for-PN5180-with-Raspberry-Pi-4/m-p/1392557#M9085</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can download Reader library for PN5180 from below link&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/designs/nfc-reader-library-software-support-for-nfc-frontend-solutions:NFC-READER-LIBRARY?tab=In-Depth_Tab" target="_blank"&gt;https://www.nxp.com/design/designs/nfc-reader-library-software-support-for-nfc-frontend-solutions:NFC-READER-LIBRARY?tab=In-Depth_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Dec 2021 07:37:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Library-for-PN5180-with-Raspberry-Pi-4/m-p/1392557#M9085</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2021-12-28T07:37:34Z</dc:date>
    </item>
    <item>
      <title>Re: Library for PN5180 with Raspberry Pi 4</title>
      <link>https://community.nxp.com/t5/NFC/Library-for-PN5180-with-Raspberry-Pi-4/m-p/1752917#M10951</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/369"&gt;@danielchen&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;which libs should we download, because the contents of the SW352236 folder do not work on raspbian. Lots of inclusion is missing. Can you directly provide a link to a C++ header to use the PN5180-nfc reader. Do you have an example without a GUI?&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;</description>
      <pubDate>Mon, 06 Nov 2023 15:46:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Library-for-PN5180-with-Raspberry-Pi-4/m-p/1752917#M10951</guid>
      <dc:creator>fy</dc:creator>
      <dc:date>2023-11-06T15:46:10Z</dc:date>
    </item>
  </channel>
</rss>