<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: How to program example code to PN7462 board</title>
    <link>https://community.nxp.com/t5/NFC/How-to-program-example-code-to-PN7462-board/m-p/1744531#M10894</link>
    <description>&lt;P&gt;Hi Daniel, Fabian (who has helped me to finalize this board), Thanks a lot and lot. It worked and I am able to download the code to board and also run some of the examples. In fact I am having a customized card and I am able to communicate to it. Thanks again a lot.&lt;/P&gt;&lt;P&gt;Couple of questions - more from understanding and clearing my doubts.&lt;/P&gt;&lt;P&gt;1. Currently there are so many project folders - I am using&amp;nbsp;PN7462AU_ex_phExMain_mcux project (which is inside phExMain). I am using contact card - and I thought phExCT7816 to be used - but this project itself has those calls - but inside&amp;nbsp;phExMain_Ct.c. So 7816 and CT cards are different (I thought contact card is always 7816 card).&lt;/P&gt;&lt;P&gt;2. When do we use&amp;nbsp;phExCT7816/ phExCTEMVCo/ phExCt explicitly? Or are these projects are there for references and&amp;nbsp;PN7462AU_ex_phExMain_mcux (inside phExMain) is the overall example of using all these different possible cards?&lt;/P&gt;&lt;P&gt;3. Is there any document (or guide) to understand these different variety of cards (so that I can propose which card to be used for particular use case)? I just googled it - seems there are lot of data - but if you have any suggestion for layman like me - it would be easy to start at some source.&lt;/P&gt;&lt;P&gt;4. Also is there any way I can create a independent project and pull in only required capabilities (just to reduce the ROM size) - may be without using RTOS (again to save the ROM). If you have these kind of details handy - please pass it on.&lt;/P&gt;&lt;P&gt;Thanks again and your replies are very useful to me.&lt;/P&gt;&lt;P&gt;With best regards,&lt;/P&gt;&lt;P&gt;//P&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 23 Oct 2023 13:25:46 GMT</pubDate>
    <dc:creator>phanids</dc:creator>
    <dc:date>2023-10-23T13:25:46Z</dc:date>
    <item>
      <title>How to program example code to PN7462 board</title>
      <link>https://community.nxp.com/t5/NFC/How-to-program-example-code-to-PN7462-board/m-p/1739809#M10863</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Seems I am missing something basic - and any of your suggestion would help me a lot.&lt;/P&gt;&lt;P&gt;I have recently purchased OM27462CDKP development kit. Downloaded the FW and SW full examples from&amp;nbsp;&lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/nfc-controller-development-kit:OM27462CDKP" target="_blank" rel="noopener"&gt;https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/nfc-controller-development-kit:OM27462CDKP &amp;nbsp;&lt;/A&gt;installed MCU Expresso and imported these example files, and build all - it looks like as below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="phanids_0-1697299861317.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/245118i0306F45E5AEB7096/image-size/medium?v=v2&amp;amp;px=400" role="button" title="phanids_0-1697299861317.png" alt="phanids_0-1697299861317.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Now I am stuck on&lt;/P&gt;&lt;P&gt;a. Which file I need to download to the board&lt;/P&gt;&lt;P&gt;b. How to download the code&lt;/P&gt;&lt;P&gt;My configuration looks as below&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="phanids_1-1697300363435.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/245119i61B1D70085C932B5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="phanids_1-1697300363435.png" alt="phanids_1-1697300363435.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;when I try to run the code by clicking on green "Play" button in the IDE, I get below errors.&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;Error starting process.&lt;/P&gt;&lt;P&gt;Cannot run program "...\NxpNfcRdLib_PN7462_v06.10.00_Pub\ExamplesPN7462AU\phExMain\mcux\DebugPN7462AU\PN7462AU_ex_phExMain_mcux.axf": Launching failed&lt;/P&gt;&lt;P&gt;Cannot run program "...\NxpNfcRdLib_PN7462_v06.10.00_Pub\ExamplesPN7462AU\phExMain\mcux\DebugPN7462AU\PN7462AU_ex_phExMain_mcux.axf": Launching failed&lt;/P&gt;&lt;P&gt;Cannot run program "....\NxpNfcRdLib_PN7462_v06.10.00_Pub\ExamplesPN7462AU\phExMain\mcux\DebugPN7462AU\PN7462AU_ex_phExMain_mcux.axf": Launching failed&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;Basically my requirement is to send some APDU commands and accordingly set some LED's.&lt;/P&gt;&lt;P&gt;With best regards,&lt;/P&gt;&lt;P&gt;//P&lt;/P&gt;</description>
      <pubDate>Sat, 14 Oct 2023 16:26:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/How-to-program-example-code-to-PN7462-board/m-p/1739809#M10863</guid>
      <dc:creator>phanids</dc:creator>
      <dc:date>2023-10-14T16:26:41Z</dc:date>
    </item>
    <item>
      <title>Re: How to program example code to PN7462 board</title>
      <link>https://community.nxp.com/t5/NFC/How-to-program-example-code-to-PN7462-board/m-p/1739919#M10866</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222324"&gt;@phanids&lt;/a&gt;&amp;nbsp;:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For downloading a project, I would suggest you use a MCU PRO link or LPC-LINK 2 , please refer to AN 11022.&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;section 5.5&amp;nbsp; Running and debugging a project&lt;/P&gt;
&lt;P&gt;Though this application note for RC663, it also applies to PN7462&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN11022.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN11022.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 16 Oct 2023 02:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/How-to-program-example-code-to-PN7462-board/m-p/1739919#M10866</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2023-10-16T02:53:46Z</dc:date>
    </item>
    <item>
      <title>Re: How to program example code to PN7462 board</title>
      <link>https://community.nxp.com/t5/NFC/How-to-program-example-code-to-PN7462-board/m-p/1744531#M10894</link>
      <description>&lt;P&gt;Hi Daniel, Fabian (who has helped me to finalize this board), Thanks a lot and lot. It worked and I am able to download the code to board and also run some of the examples. In fact I am having a customized card and I am able to communicate to it. Thanks again a lot.&lt;/P&gt;&lt;P&gt;Couple of questions - more from understanding and clearing my doubts.&lt;/P&gt;&lt;P&gt;1. Currently there are so many project folders - I am using&amp;nbsp;PN7462AU_ex_phExMain_mcux project (which is inside phExMain). I am using contact card - and I thought phExCT7816 to be used - but this project itself has those calls - but inside&amp;nbsp;phExMain_Ct.c. So 7816 and CT cards are different (I thought contact card is always 7816 card).&lt;/P&gt;&lt;P&gt;2. When do we use&amp;nbsp;phExCT7816/ phExCTEMVCo/ phExCt explicitly? Or are these projects are there for references and&amp;nbsp;PN7462AU_ex_phExMain_mcux (inside phExMain) is the overall example of using all these different possible cards?&lt;/P&gt;&lt;P&gt;3. Is there any document (or guide) to understand these different variety of cards (so that I can propose which card to be used for particular use case)? I just googled it - seems there are lot of data - but if you have any suggestion for layman like me - it would be easy to start at some source.&lt;/P&gt;&lt;P&gt;4. Also is there any way I can create a independent project and pull in only required capabilities (just to reduce the ROM size) - may be without using RTOS (again to save the ROM). If you have these kind of details handy - please pass it on.&lt;/P&gt;&lt;P&gt;Thanks again and your replies are very useful to me.&lt;/P&gt;&lt;P&gt;With best regards,&lt;/P&gt;&lt;P&gt;//P&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Oct 2023 13:25:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/How-to-program-example-code-to-PN7462-board/m-p/1744531#M10894</guid>
      <dc:creator>phanids</dc:creator>
      <dc:date>2023-10-23T13:25:46Z</dc:date>
    </item>
  </channel>
</rss>