<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SetConfiguration Command length error ntag 424 in NFC</title>
    <link>https://community.nxp.com/t5/NFC/SetConfiguration-Command-length-error-ntag-424/m-p/1742130#M10873</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to run setConfiguration command and according to NT4H2421Gx PDF the command should be like : [ 0x90,0x5C,0x00,0x00,&lt;FONT color="#339966"&gt;0x06&lt;/FONT&gt;,&lt;FONT color="#0000FF"&gt;0x0A&lt;/FONT&gt;,&lt;FONT color="#FF0000"&gt;0x00&lt;/FONT&gt;,0x00,0x00,0x00,0x00,0x00]&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;&lt;FONT color="#339966"&gt;Lc 0x06 : Data Parameters length is 5 + &lt;FONT color="#0000FF"&gt;1 (option = 0x0A)&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;Option : 0x0A =&amp;gt; Failed authentication counter setting&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;Data (FailedCtrOption) : 0x00 =&amp;gt; it 0: Set to 0b for disabling&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;&lt;STRONG&gt;but it return 7Eh&lt;/STRONG&gt; (Option 0Ah: Data length is not 5) while is 5 !&lt;/FONT&gt;&lt;/P&gt;&lt;DIV&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Any help appreciated.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/DIV&gt;</description>
    <pubDate>Wed, 18 Oct 2023 13:35:20 GMT</pubDate>
    <dc:creator>zahra2023</dc:creator>
    <dc:date>2023-10-18T13:35:20Z</dc:date>
    <item>
      <title>SetConfiguration Command length error ntag 424</title>
      <link>https://community.nxp.com/t5/NFC/SetConfiguration-Command-length-error-ntag-424/m-p/1742130#M10873</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to run setConfiguration command and according to NT4H2421Gx PDF the command should be like : [ 0x90,0x5C,0x00,0x00,&lt;FONT color="#339966"&gt;0x06&lt;/FONT&gt;,&lt;FONT color="#0000FF"&gt;0x0A&lt;/FONT&gt;,&lt;FONT color="#FF0000"&gt;0x00&lt;/FONT&gt;,0x00,0x00,0x00,0x00,0x00]&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;&lt;FONT color="#339966"&gt;Lc 0x06 : Data Parameters length is 5 + &lt;FONT color="#0000FF"&gt;1 (option = 0x0A)&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;Option : 0x0A =&amp;gt; Failed authentication counter setting&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;Data (FailedCtrOption) : 0x00 =&amp;gt; it 0: Set to 0b for disabling&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;&lt;STRONG&gt;but it return 7Eh&lt;/STRONG&gt; (Option 0Ah: Data length is not 5) while is 5 !&lt;/FONT&gt;&lt;/P&gt;&lt;DIV&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Any help appreciated.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 18 Oct 2023 13:35:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/SetConfiguration-Command-length-error-ntag-424/m-p/1742130#M10873</guid>
      <dc:creator>zahra2023</dc:creator>
      <dc:date>2023-10-18T13:35:20Z</dc:date>
    </item>
  </channel>
</rss>