<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックAbout RF collision avoidance</title>
    <link>https://community.nxp.com/t5/NFC/About-RF-collision-avoidance/m-p/1721557#M10728</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using PN5190. I want to know about RF collision avoidance.&lt;BR /&gt;The setting (PHHAL_HW_CONFIG_RFCA) can be set by phNfcLib_SetConfig().&lt;/P&gt;&lt;P&gt;Checking the NFC Reader Library, the default is PH_ON, which is set during initialization: phhalHw_Pn5190_Init() and phhalHw_Pn5190_DeInit().&lt;BR /&gt;And in phacDiscLoop_Run, it sets PH_ON for NFC/ISO and PH_OFF for EMV.&lt;/P&gt;&lt;P&gt;[Question 1]&lt;BR /&gt;If the default is changed to PH_OFF and PH_OFF is set for NFC/ISO in phacDiscLoop_Run,&lt;BR /&gt;will there be any impact on some movements? Will it only not detect collision errors during carrier on?&lt;/P&gt;&lt;P&gt;[Question 2]&lt;BR /&gt;The default setting is PH_ON, and it is only changed to PH_OFF for EMV.&lt;BR /&gt;Is there any reason for changing EMV setting?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 13 Sep 2023 02:42:39 GMT</pubDate>
    <dc:creator>ttkk_01</dc:creator>
    <dc:date>2023-09-13T02:42:39Z</dc:date>
    <item>
      <title>About RF collision avoidance</title>
      <link>https://community.nxp.com/t5/NFC/About-RF-collision-avoidance/m-p/1721557#M10728</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using PN5190. I want to know about RF collision avoidance.&lt;BR /&gt;The setting (PHHAL_HW_CONFIG_RFCA) can be set by phNfcLib_SetConfig().&lt;/P&gt;&lt;P&gt;Checking the NFC Reader Library, the default is PH_ON, which is set during initialization: phhalHw_Pn5190_Init() and phhalHw_Pn5190_DeInit().&lt;BR /&gt;And in phacDiscLoop_Run, it sets PH_ON for NFC/ISO and PH_OFF for EMV.&lt;/P&gt;&lt;P&gt;[Question 1]&lt;BR /&gt;If the default is changed to PH_OFF and PH_OFF is set for NFC/ISO in phacDiscLoop_Run,&lt;BR /&gt;will there be any impact on some movements? Will it only not detect collision errors during carrier on?&lt;/P&gt;&lt;P&gt;[Question 2]&lt;BR /&gt;The default setting is PH_ON, and it is only changed to PH_OFF for EMV.&lt;BR /&gt;Is there any reason for changing EMV setting?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 13 Sep 2023 02:42:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/About-RF-collision-avoidance/m-p/1721557#M10728</guid>
      <dc:creator>ttkk_01</dc:creator>
      <dc:date>2023-09-13T02:42:39Z</dc:date>
    </item>
  </channel>
</rss>