<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックPN5180 SPI from esp32 core (Arduino ide) takes too long</title>
    <link>https://community.nxp.com/t5/NFC/PN5180-SPI-from-esp32-core-Arduino-ide-takes-too-long/m-p/1645972#M10314</link>
    <description>&lt;P&gt;Hi, I implemented an iso15693 inventory16 command on an esp32 controller using Arduino IDE.&lt;/P&gt;&lt;P&gt;It works well, although collisions happen. But i had to delay flow control 1ms after asserting NSS before wait for busy pin high. If i didnt that it doesn't work.&lt;/P&gt;&lt;P&gt;The problem Is the inventory take almost a second for few tags. This Is a long time for my application.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried microsecondsDelay with values under 1000us, but it didn't work either, inventory fails.&lt;/P&gt;&lt;P&gt;Pn5180 datasheet say nothing about this. Has anyone had this problem?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help. Thanks in Advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 07 May 2023 04:57:09 GMT</pubDate>
    <dc:creator>oferrer</dc:creator>
    <dc:date>2023-05-07T04:57:09Z</dc:date>
    <item>
      <title>PN5180 SPI from esp32 core (Arduino ide) takes too long</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-SPI-from-esp32-core-Arduino-ide-takes-too-long/m-p/1645972#M10314</link>
      <description>&lt;P&gt;Hi, I implemented an iso15693 inventory16 command on an esp32 controller using Arduino IDE.&lt;/P&gt;&lt;P&gt;It works well, although collisions happen. But i had to delay flow control 1ms after asserting NSS before wait for busy pin high. If i didnt that it doesn't work.&lt;/P&gt;&lt;P&gt;The problem Is the inventory take almost a second for few tags. This Is a long time for my application.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried microsecondsDelay with values under 1000us, but it didn't work either, inventory fails.&lt;/P&gt;&lt;P&gt;Pn5180 datasheet say nothing about this. Has anyone had this problem?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help. Thanks in Advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 07 May 2023 04:57:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-SPI-from-esp32-core-Arduino-ide-takes-too-long/m-p/1645972#M10314</guid>
      <dc:creator>oferrer</dc:creator>
      <dc:date>2023-05-07T04:57:09Z</dc:date>
    </item>
  </channel>
</rss>