<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 PN7160 current draw in Card Emulation</title>
    <link>https://community.nxp.com/t5/NFC/PN7160-current-draw-in-Card-Emulation/m-p/1634822#M10238</link>
    <description>&lt;P&gt;I'm contemplating using the PN7160 in a field-powered Card Emulation role using a low-power microcontroller as the host.&amp;nbsp; I'm confused with the datasheet that has two Ibat sections and none of the entries seem to clearly apply.&amp;nbsp; I understand to talk to a host, the Vdd(pad) must be present, and this would indicate Full-Power Mode (per section 11.1.1).&amp;nbsp; I am thinking that the power state (11.1.2) would be Active, and the device is operating as a Listener.&amp;nbsp; Therefore, the closest scenario might be "Idle and Target Active" state in Table 35 - 4.55mA typ.&lt;/P&gt;&lt;P&gt;Is there a clear "right" answer?&lt;/P&gt;</description>
    <pubDate>Mon, 17 Apr 2023 17:58:43 GMT</pubDate>
    <dc:creator>dlormand</dc:creator>
    <dc:date>2023-04-17T17:58:43Z</dc:date>
    <item>
      <title>PN7160 current draw in Card Emulation</title>
      <link>https://community.nxp.com/t5/NFC/PN7160-current-draw-in-Card-Emulation/m-p/1634822#M10238</link>
      <description>&lt;P&gt;I'm contemplating using the PN7160 in a field-powered Card Emulation role using a low-power microcontroller as the host.&amp;nbsp; I'm confused with the datasheet that has two Ibat sections and none of the entries seem to clearly apply.&amp;nbsp; I understand to talk to a host, the Vdd(pad) must be present, and this would indicate Full-Power Mode (per section 11.1.1).&amp;nbsp; I am thinking that the power state (11.1.2) would be Active, and the device is operating as a Listener.&amp;nbsp; Therefore, the closest scenario might be "Idle and Target Active" state in Table 35 - 4.55mA typ.&lt;/P&gt;&lt;P&gt;Is there a clear "right" answer?&lt;/P&gt;</description>
      <pubDate>Mon, 17 Apr 2023 17:58:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7160-current-draw-in-Card-Emulation/m-p/1634822#M10238</guid>
      <dc:creator>dlormand</dc:creator>
      <dc:date>2023-04-17T17:58:43Z</dc:date>
    </item>
  </channel>
</rss>