<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 Consultation on PN7160 certification issues</title>
    <link>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1631652#M10221</link>
    <description>&lt;P&gt;&lt;SPAN class=""&gt;Hi NXP,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Can&amp;nbsp; PN7160 support EMV L1, paypass, and paywave?&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;thank you.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 12 Apr 2023 02:02:50 GMT</pubDate>
    <dc:creator>Karyliu</dc:creator>
    <dc:date>2023-04-12T02:02:50Z</dc:date>
    <item>
      <title>Consultation on PN7160 certification issues</title>
      <link>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1631652#M10221</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;Hi NXP,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Can&amp;nbsp; PN7160 support EMV L1, paypass, and paywave?&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;thank you.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Apr 2023 02:02:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1631652#M10221</guid>
      <dc:creator>Karyliu</dc:creator>
      <dc:date>2023-04-12T02:02:50Z</dc:date>
    </item>
    <item>
      <title>Re: Consultation on PN7160 certification issues</title>
      <link>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1631710#M10224</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198313"&gt;@Karyliu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;PN7160 is not targeted for EMVCo products.&amp;nbsp; PN7160 is an NFC controller designed for integration in mobile devices and devices compliant with NFC standards.&amp;nbsp; Applications includes Mobile devices, portable equipment, consumer devices...&lt;/P&gt;
&lt;P&gt;For EMVCo products. I would suggest you use PN5190.&amp;nbsp; PN5190 is a robust solution for payment terminals. Offering full compliance with EMVCo 3.1 and NFC Forum certifications.&lt;/P&gt;
&lt;P&gt;please refer to below link for more details about PN5190.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/nfc-frontend-supporting-challenging-rf-environment-for-payment-physical-access-control:PN5190" target="_blank"&gt;https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/nfc-frontend-supporting-challenging-rf-environment-for-payment-physical-access-control:PN5190&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Apr 2023 04:08:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1631710#M10224</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2023-04-12T04:08:10Z</dc:date>
    </item>
    <item>
      <title>Re: Consultation on PN7160 certification issues</title>
      <link>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1631856#M10225</link>
      <description>&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thank you for your reply.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;What system versions are supported by PN5190?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Currently, Android 13 and above versions are required. Can PN5190 support it?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Apr 2023 06:51:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1631856#M10225</guid>
      <dc:creator>Karyliu</dc:creator>
      <dc:date>2023-04-12T06:51:59Z</dc:date>
    </item>
    <item>
      <title>Re: Consultation on PN7160 certification issues</title>
      <link>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1632161#M10226</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198313"&gt;@Karyliu&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I just want to add something to the answer of Daniel.&lt;/P&gt;
&lt;P&gt;Yes, the PN5190 is tailored for EMVCo usecase and fits it perfectly. But it is only a NFC Front-End and needs a host controller where the application runs. This is different from a PN7160 which is a controller itself running NCI for an interface.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The better suited successor of the PN7160 would be the upcoming PN7220. Which is also targeting the EMVCo marked and supporting Android 13. Unfortunately it is not released yet and the official release date is around June.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards, Alex&lt;/P&gt;</description>
      <pubDate>Wed, 12 Apr 2023 13:02:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1632161#M10226</guid>
      <dc:creator>AlexanderB</dc:creator>
      <dc:date>2023-04-12T13:02:10Z</dc:date>
    </item>
    <item>
      <title>Re: Consultation on PN7160 certification issues</title>
      <link>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1632691#M10227</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/369"&gt;@danielchen&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/124376"&gt;@AlexanderB&lt;/a&gt;&amp;nbsp;What about for the use case of using something like Felix Cloud Kernel for payment processing?&amp;nbsp; Requirements there are only to have the hardware be EMV L1 certified, no need for L2/L3 certification.&amp;nbsp; Would the PN7160, PN7642 or even the PN7462 (legacy product?) work in this situation?&amp;nbsp; Linux based system would be the go-between the cloud and the MCU/integrated front end. Our preferred part would be the PN7642, but it isn't clear if that part has/can achieve EMVL1 certification.&lt;/P&gt;&lt;P&gt;Are samples available for the PN7220?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Apr 2023 02:34:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1632691#M10227</guid>
      <dc:creator>JohnEE123</dc:creator>
      <dc:date>2023-04-13T02:34:12Z</dc:date>
    </item>
    <item>
      <title>Re: Consultation on PN7160 certification issues</title>
      <link>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1632854#M10228</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/215728"&gt;@JohnEE123&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Unfortunately I am not familiar with the Felix Cloud Kernel and cannot comment on this.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The PN7160 can hardly pass EMV L1 (and is not recommended for new EMV designs), it heavily depends on the sorrounding material. You are far better of with a PN5190 or PN7642.&amp;nbsp;&lt;BR /&gt;The PN7642 and PN5190 share the same analog front-end. Even though the PN76 family is not placed in the EMV marked by us, we are very confindent that it can pass EMV L1 (as the PN5190 does).&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For the PN7220 currently are no samples available. I do not know the timeline when engineering samples will be made available.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Greetings, Alex&lt;/P&gt;</description>
      <pubDate>Thu, 13 Apr 2023 06:43:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1632854#M10228</guid>
      <dc:creator>AlexanderB</dc:creator>
      <dc:date>2023-04-13T06:43:47Z</dc:date>
    </item>
    <item>
      <title>Re: Consultation on PN7160 certification issues</title>
      <link>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1685252#M10549</link>
      <description>&lt;P&gt;Hi AlexanderB,&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Have pN7220 been released yet?&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;I have information on the NXP official website.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Can PN7220 pass PCI certification?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Does PN7160 support PCI authentication?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jul 2023 01:53:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1685252#M10549</guid>
      <dc:creator>Karyliu</dc:creator>
      <dc:date>2023-07-11T01:53:56Z</dc:date>
    </item>
    <item>
      <title>Re: Consultation on PN7160 certification issues</title>
      <link>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1686722#M10563</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198313"&gt;@Karyliu&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;The PN7220 has been released:&amp;nbsp;&lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/emv-l1-compliant-nfc-controller-with-nci-interface-supporting-emv-and-nfc-forum-applications:PN7220" target="_self"&gt;PN7220&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The PCI certification is done for the POS terminal and not a single chip. To be PCI compliant you need a secure host microcontroller.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The PN7160 is not targeting the POS market.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Alexander&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 14:16:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1686722#M10563</guid>
      <dc:creator>AlexanderB</dc:creator>
      <dc:date>2023-07-12T14:16:24Z</dc:date>
    </item>
    <item>
      <title>Re: Consultation on PN7160 certification issues</title>
      <link>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1686954#M10569</link>
      <description>&lt;P&gt;Hi Alexander,&lt;/P&gt;&lt;P&gt;I got it.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jul 2023 01:14:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Consultation-on-PN7160-certification-issues/m-p/1686954#M10569</guid>
      <dc:creator>Karyliu</dc:creator>
      <dc:date>2023-07-13T01:14:00Z</dc:date>
    </item>
  </channel>
</rss>