<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックPN7150 nfcDemoApp poll Crash</title>
    <link>https://community.nxp.com/t5/NFC/PN7150-nfcDemoApp-poll-Crash/m-p/1625168#M10178</link>
    <description>&lt;P&gt;I use Raspberry 3B &amp;amp;&amp;nbsp;OM5579/PN7150RPI run the demo "nfcDemoApp poll " follow&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/Easy-set-up-of-NFC-on-Raspberry-Pi/ta-p/1099034" target="_blank"&gt;Easy set-up of NFC on Raspberry Pi - NXP Community&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Usually works normally，But when I put 2 MIFARE Classic cards into the field at the same time many times in a row, it crashed.&lt;/P&gt;&lt;P&gt;(&lt;/P&gt;&lt;P&gt;it’s ok when put 2 NTAG213 cards into the field at the same time many times in a row;&lt;/P&gt;&lt;P&gt;it’s ok when put only one MIFARE Classic card into the field at the same time many times in a row;&lt;/P&gt;&lt;P&gt;)&lt;/P&gt;&lt;P&gt;Why?&amp;nbsp;There are logs here, please help analyze them ,Thanks!&lt;/P&gt;</description>
    <pubDate>Thu, 30 Mar 2023 09:41:10 GMT</pubDate>
    <dc:creator>ethan_dang1</dc:creator>
    <dc:date>2023-03-30T09:41:10Z</dc:date>
    <item>
      <title>PN7150 nfcDemoApp poll Crash</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-nfcDemoApp-poll-Crash/m-p/1625168#M10178</link>
      <description>&lt;P&gt;I use Raspberry 3B &amp;amp;&amp;nbsp;OM5579/PN7150RPI run the demo "nfcDemoApp poll " follow&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/Easy-set-up-of-NFC-on-Raspberry-Pi/ta-p/1099034" target="_blank"&gt;Easy set-up of NFC on Raspberry Pi - NXP Community&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Usually works normally，But when I put 2 MIFARE Classic cards into the field at the same time many times in a row, it crashed.&lt;/P&gt;&lt;P&gt;(&lt;/P&gt;&lt;P&gt;it’s ok when put 2 NTAG213 cards into the field at the same time many times in a row;&lt;/P&gt;&lt;P&gt;it’s ok when put only one MIFARE Classic card into the field at the same time many times in a row;&lt;/P&gt;&lt;P&gt;)&lt;/P&gt;&lt;P&gt;Why?&amp;nbsp;There are logs here, please help analyze them ,Thanks!&lt;/P&gt;</description>
      <pubDate>Thu, 30 Mar 2023 09:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-nfcDemoApp-poll-Crash/m-p/1625168#M10178</guid>
      <dc:creator>ethan_dang1</dc:creator>
      <dc:date>2023-03-30T09:41:10Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 nfcDemoApp poll Crash</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-nfcDemoApp-poll-Crash/m-p/1625711#M10183</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214798"&gt;@ethan_dang1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for sharing and contacting us. Based on your description I'd like to know why do you put two mifare classic cards on the field at the same and&amp;nbsp;does your application scenario have to be like this?&amp;nbsp;I want to know this because I need to make sure if the Demo supports this application scenario.&lt;BR /&gt;&lt;BR /&gt;To update this case, you may reply by email.&lt;BR /&gt;To provide confidential information or attachments, you may add that online.&lt;BR /&gt;&lt;BR /&gt;Please login to our NXP technical support portal:&lt;BR /&gt;&lt;A href="https://support.nxp.com/s/case/5002p00002s4gPIAAY" data-cke-saved-href="https://support.nxp.com/s/case/5002p00002s4gPIAAY" target="_blank"&gt;https://support.nxp.com/s/case/5002p00002s4gPIAAY&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;The portal allows access to the full details of the case, including the previous communication.&lt;BR /&gt;&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Kelly&lt;BR /&gt;Technical Support&lt;BR /&gt;NXP Semiconductor&lt;/P&gt;</description>
      <pubDate>Fri, 31 Mar 2023 02:35:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-nfcDemoApp-poll-Crash/m-p/1625711#M10183</guid>
      <dc:creator>KaiLi</dc:creator>
      <dc:date>2023-03-31T02:35:50Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 nfcDemoApp poll Crash</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-nfcDemoApp-poll-Crash/m-p/1625789#M10185</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Kelly&lt;/SPAN&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205266"&gt;@KaiLi&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Put two mifare classic cards on the field at the same because it happens sometimes(.e.g Multiple cards in the wallet,just put wallet directly into the field)&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 31 Mar 2023 05:35:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-nfcDemoApp-poll-Crash/m-p/1625789#M10185</guid>
      <dc:creator>ethan_dang1</dc:creator>
      <dc:date>2023-03-31T05:35:55Z</dc:date>
    </item>
  </channel>
</rss>