<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックPN7160 matching with DPC</title>
    <link>https://community.nxp.com/t5/NFC/PN7160-matching-with-DPC/m-p/1602009#M10045</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;According to the antenna matching guide, asymmetric matching is used for the OM27160 demo board (fr0 = 22MHz).&lt;/P&gt;&lt;P&gt;According to the circuit diagram for the demo board, the filter frequency is 14.5MHz (160nH, 750pF), so symmetrical is used which, according to the antenna matching guide, requires DPC ?&lt;BR /&gt;&lt;BR /&gt;In the source code (I use the MCUXpresso library) nothing indicates that DPC is used.&lt;/P&gt;&lt;P&gt;Does the demo project use DPC and what filter value is recommended?&lt;/P&gt;&lt;P&gt;I designed and calculated my own board with a slightly larger antenna and achieve extremely poor results with a fr0 with 22MHz and only passable with 14.5MHz.&lt;/P&gt;&lt;P&gt;The antenna data was determined with a network analyzer, the matching circuit with the online tool and the PN7160 matching calculator.&lt;/P&gt;&lt;P&gt;Where can I start to get better results? (Increase Q, increase fr0, ...)&lt;/P&gt;&lt;P&gt;How can I restore the default values ​​of the NxpNci_RF_CONF? The default values ​​are not mentioned in the UM.&lt;/P&gt;&lt;P&gt;Thanks very much,&lt;BR /&gt;Michael&lt;/P&gt;</description>
    <pubDate>Mon, 20 Feb 2023 12:58:39 GMT</pubDate>
    <dc:creator>michael_d_1983</dc:creator>
    <dc:date>2023-02-20T12:58:39Z</dc:date>
    <item>
      <title>PN7160 matching with DPC</title>
      <link>https://community.nxp.com/t5/NFC/PN7160-matching-with-DPC/m-p/1602009#M10045</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;According to the antenna matching guide, asymmetric matching is used for the OM27160 demo board (fr0 = 22MHz).&lt;/P&gt;&lt;P&gt;According to the circuit diagram for the demo board, the filter frequency is 14.5MHz (160nH, 750pF), so symmetrical is used which, according to the antenna matching guide, requires DPC ?&lt;BR /&gt;&lt;BR /&gt;In the source code (I use the MCUXpresso library) nothing indicates that DPC is used.&lt;/P&gt;&lt;P&gt;Does the demo project use DPC and what filter value is recommended?&lt;/P&gt;&lt;P&gt;I designed and calculated my own board with a slightly larger antenna and achieve extremely poor results with a fr0 with 22MHz and only passable with 14.5MHz.&lt;/P&gt;&lt;P&gt;The antenna data was determined with a network analyzer, the matching circuit with the online tool and the PN7160 matching calculator.&lt;/P&gt;&lt;P&gt;Where can I start to get better results? (Increase Q, increase fr0, ...)&lt;/P&gt;&lt;P&gt;How can I restore the default values ​​of the NxpNci_RF_CONF? The default values ​​are not mentioned in the UM.&lt;/P&gt;&lt;P&gt;Thanks very much,&lt;BR /&gt;Michael&lt;/P&gt;</description>
      <pubDate>Mon, 20 Feb 2023 12:58:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7160-matching-with-DPC/m-p/1602009#M10045</guid>
      <dc:creator>michael_d_1983</dc:creator>
      <dc:date>2023-02-20T12:58:39Z</dc:date>
    </item>
    <item>
      <title>Re: PN7160 matching with DPC</title>
      <link>https://community.nxp.com/t5/NFC/PN7160-matching-with-DPC/m-p/1609916#M10075</link>
      <description>&lt;P&gt;How can I restore the default values ​​of the NxpNci_RF_CONF? The default values ​​are not mentioned in the UM.&lt;/P&gt;&lt;P&gt;Thanks very much,&lt;BR /&gt;Michael&lt;/P&gt;</description>
      <pubDate>Mon, 06 Mar 2023 09:43:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7160-matching-with-DPC/m-p/1609916#M10075</guid>
      <dc:creator>michael_d_1983</dc:creator>
      <dc:date>2023-03-06T09:43:12Z</dc:date>
    </item>
  </channel>
</rss>