<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NavQ 8MMNavQ Discussion中的主题 Re: Compatibility of Raspberry pi Official 7 inch LCD With NavQ</title>
    <link>https://community.nxp.com/t5/NavQ-8MMNavQ-Discussion/Compatibility-of-Raspberry-pi-Official-7-inch-LCD-With-NavQ/m-p/1216921#M41</link>
    <description>&lt;P&gt;For powering external peripherals - beyond what the on board USB-C power supply can handle - you can use a powered USB hub. That will offload the power of a keyboard and mouse to the powered hub adapter.&lt;BR /&gt;&lt;BR /&gt;If you are asking how to power the NavQ, then you can use a USB-C input for power. or apply up to 20V on the power input connector header.&lt;/P&gt;
&lt;P&gt;see &lt;A href="https://nxp.gitbook.io/8mmnavq" target="_blank"&gt;https://nxp.gitbook.io/8mmnavq&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 19 Jan 2021 13:46:18 GMT</pubDate>
    <dc:creator>iaingalloway</dc:creator>
    <dc:date>2021-01-19T13:46:18Z</dc:date>
    <item>
      <title>Compatibility of Raspberry pi Official 7 inch LCD With NavQ</title>
      <link>https://community.nxp.com/t5/NavQ-8MMNavQ-Discussion/Compatibility-of-Raspberry-pi-Official-7-inch-LCD-With-NavQ/m-p/1189281#M39</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is the&amp;nbsp;Raspberry pi Official 7 inch LCD compatible with NavQ? Can you also specify any adapter for external supply to the NavQ with connected peripherals (keyboard, etc.)?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I appreciate any help you can provide.&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Nilanjan&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 21:27:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NavQ-8MMNavQ-Discussion/Compatibility-of-Raspberry-pi-Official-7-inch-LCD-With-NavQ/m-p/1189281#M39</guid>
      <dc:creator>nilz</dc:creator>
      <dc:date>2020-11-25T21:27:53Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility of Raspberry pi Official 7 inch LCD With NavQ</title>
      <link>https://community.nxp.com/t5/NavQ-8MMNavQ-Discussion/Compatibility-of-Raspberry-pi-Official-7-inch-LCD-With-NavQ/m-p/1216920#M40</link>
      <description>&lt;P&gt;Emcraft have a 7" LCD that has been tested with NavQ.&amp;nbsp;&lt;BR /&gt;Technically many other displays can be made to work, but they have not been tested or had the settings configured for them.&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jan 2021 13:43:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NavQ-8MMNavQ-Discussion/Compatibility-of-Raspberry-pi-Official-7-inch-LCD-With-NavQ/m-p/1216920#M40</guid>
      <dc:creator>iaingalloway</dc:creator>
      <dc:date>2021-01-19T13:43:31Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility of Raspberry pi Official 7 inch LCD With NavQ</title>
      <link>https://community.nxp.com/t5/NavQ-8MMNavQ-Discussion/Compatibility-of-Raspberry-pi-Official-7-inch-LCD-With-NavQ/m-p/1216921#M41</link>
      <description>&lt;P&gt;For powering external peripherals - beyond what the on board USB-C power supply can handle - you can use a powered USB hub. That will offload the power of a keyboard and mouse to the powered hub adapter.&lt;BR /&gt;&lt;BR /&gt;If you are asking how to power the NavQ, then you can use a USB-C input for power. or apply up to 20V on the power input connector header.&lt;/P&gt;
&lt;P&gt;see &lt;A href="https://nxp.gitbook.io/8mmnavq" target="_blank"&gt;https://nxp.gitbook.io/8mmnavq&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jan 2021 13:46:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NavQ-8MMNavQ-Discussion/Compatibility-of-Raspberry-pi-Official-7-inch-LCD-With-NavQ/m-p/1216921#M41</guid>
      <dc:creator>iaingalloway</dc:creator>
      <dc:date>2021-01-19T13:46:18Z</dc:date>
    </item>
  </channel>
</rss>