<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: Writing data flash of MPC5606B through JTAG interface using Nexus.</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Writing-data-flash-of-MPC5606B-through-JTAG-interface-using/m-p/728609#M9852</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I know that UPA-S can read.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Apr 2018 14:56:21 GMT</pubDate>
    <dc:creator>danielflor</dc:creator>
    <dc:date>2018-04-06T14:56:21Z</dc:date>
    <item>
      <title>Writing data flash of MPC5606B through JTAG interface using Nexus.</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Writing-data-flash-of-MPC5606B-through-JTAG-interface-using/m-p/728607#M9850</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm programming flash memory of MPC5606B through JTAG interface using Nexus. I'm imitating a tool that perform this task. However, in the middle of the process, the entire flash memory is erased. I skipped this part in code, but, when I do this, the write to memory does not work. Of course I have a backup of the memory, but, I was wondering, to allow programming the data flash is necessary to erase a block memory? I mean, the procedure is a bit long, so, I was wondering if I can just to write in memory positions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The tool makes a selection of 4 blocks of 16kB to be erased, it is the entire dataflash of MPC5606, 64kB. So, I can erase only 16kB instead of 64kB, but, my doubt is, is really necessary to erase a block of 16kB, or the entire memory of 64kB, just to write some bytes , for example 16 bytes, in the flash memory ?&lt;/P&gt;&lt;P&gt;I looked about this information on adtasheets and documents and I didn't find nothing.&lt;/P&gt;&lt;P&gt;With my bests regards ,&lt;BR /&gt;Daniel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2018 11:44:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Writing-data-flash-of-MPC5606B-through-JTAG-interface-using/m-p/728607#M9850</guid>
      <dc:creator>danielflor</dc:creator>
      <dc:date>2018-01-16T11:44:12Z</dc:date>
    </item>
    <item>
      <title>Re: Writing data flash of MPC5606B through JTAG interface using Nexus.</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Writing-data-flash-of-MPC5606B-through-JTAG-interface-using/m-p/728608#M9851</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Daniel!&lt;/P&gt;&lt;P&gt;In common case, not necessary to erase flash before it writing. But when you access via jtag, there is no possibility to write flash directly. So you download a peace of code into cpu RAM. Then this peace of code executes secuence: erase and write...&lt;/P&gt;&lt;P&gt;Daniel, what tool are you using for access via JTAG? I am looking for such a tool for MPC5606.&lt;/P&gt;&lt;P&gt;BR!&lt;/P&gt;&lt;P&gt;Andrey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jan 2018 14:08:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Writing-data-flash-of-MPC5606B-through-JTAG-interface-using/m-p/728608#M9851</guid>
      <dc:creator>andreyabramchuk</dc:creator>
      <dc:date>2018-01-22T14:08:52Z</dc:date>
    </item>
    <item>
      <title>Re: Writing data flash of MPC5606B through JTAG interface using Nexus.</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Writing-data-flash-of-MPC5606B-through-JTAG-interface-using/m-p/728609#M9852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I know that UPA-S can read.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Apr 2018 14:56:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Writing-data-flash-of-MPC5606B-through-JTAG-interface-using/m-p/728609#M9852</guid>
      <dc:creator>danielflor</dc:creator>
      <dc:date>2018-04-06T14:56:21Z</dc:date>
    </item>
  </channel>
</rss>