<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5645S interrupt handlers</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5645S-interrupt-handlers/m-p/725502#M9772</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I would recommend to see following thread:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/358065"&gt;interrupt definition&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you cannot find enough examples for MPC5645S, I could recommend to see MPC5644A, MPC5646B or MPC5643L example using e200z4 core as well and principle or interrupt handling is the same as well:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329623"&gt;https://community.nxp.com/docs/DOC-329623&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Dec 2017 15:24:33 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2017-12-15T15:24:33Z</dc:date>
    <item>
      <title>MPC5645S interrupt handlers</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5645S-interrupt-handlers/m-p/725501#M9771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;My project use the MPC5645s.&lt;/P&gt;&lt;P&gt;I would like to code the interrut system in software or hardware mode whichever is simpler to implement.&lt;/P&gt;&lt;P&gt;I am therefore looking for some existing files that would make my task easier.&lt;/P&gt;&lt;P&gt;I have found a lot of code targeting the MPC560xs but nothing for the MPC5645s.&lt;/P&gt;&lt;P&gt;The MPC560xs are based on a e200z0 (32 bits GPRs). The MPC5645s is based on a e200z4 (64 bits GPRs)&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you know if the MPC560xs interrupt drivers can be used on the MPC5645s ? (mainly the&amp;nbsp; context saveguard/restitution file named intc_sw_handlers.s)&amp;nbsp;&lt;/P&gt;&lt;P&gt;If not, would you know where I can get the appropriate drivers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Dec 2017 10:15:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5645S-interrupt-handlers/m-p/725501#M9771</guid>
      <dc:creator>deniszallot</dc:creator>
      <dc:date>2017-12-15T10:15:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5645S interrupt handlers</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5645S-interrupt-handlers/m-p/725502#M9772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I would recommend to see following thread:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/358065"&gt;interrupt definition&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you cannot find enough examples for MPC5645S, I could recommend to see MPC5644A, MPC5646B or MPC5643L example using e200z4 core as well and principle or interrupt handling is the same as well:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329623"&gt;https://community.nxp.com/docs/DOC-329623&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Dec 2017 15:24:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5645S-interrupt-handlers/m-p/725502#M9772</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2017-12-15T15:24:33Z</dc:date>
    </item>
  </channel>
</rss>