<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5777C-Clock source to the PIT Timer in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5777C-Clock-source-to-the-PIT-Timer/m-p/725492#M9769</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;clocks are configured in the startup, see init.s file.&lt;/P&gt;&lt;P&gt;PLL0 is configured to 192MHz (40MHz XOSC reference) and PLL1 to 264MHz (48MHz PLL0 PHI1 output reference).&lt;/P&gt;&lt;P&gt;PIT is running from PER_CLK; as the setting used is SIU_SYSDIV[PERCLKSEL]=1 and SIU_SYSDIV[PERDIV]=0, the&lt;/P&gt;&lt;P&gt;PIT clock is PLL0/2 = 96MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 May 2018 10:54:10 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2018-05-28T10:54:10Z</dc:date>
    <item>
      <title>MPC5777C-Clock source to the PIT Timer</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777C-Clock-source-to-the-PIT-Timer/m-p/725491#M9768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-328290"&gt;Example MPC5777C-PinToggleStationery GHS714&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for this example,could you help me about the clock source to the PIT Timer .&lt;/P&gt;&lt;P&gt;what is the out put clock friquency of phi and phi1 in above example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please help on .&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 27 May 2018 07:33:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777C-Clock-source-to-the-PIT-Timer/m-p/725491#M9768</guid>
      <dc:creator>yashkumar</dc:creator>
      <dc:date>2018-05-27T07:33:59Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777C-Clock source to the PIT Timer</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777C-Clock-source-to-the-PIT-Timer/m-p/725492#M9769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;clocks are configured in the startup, see init.s file.&lt;/P&gt;&lt;P&gt;PLL0 is configured to 192MHz (40MHz XOSC reference) and PLL1 to 264MHz (48MHz PLL0 PHI1 output reference).&lt;/P&gt;&lt;P&gt;PIT is running from PER_CLK; as the setting used is SIU_SYSDIV[PERCLKSEL]=1 and SIU_SYSDIV[PERDIV]=0, the&lt;/P&gt;&lt;P&gt;PIT clock is PLL0/2 = 96MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 May 2018 10:54:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777C-Clock-source-to-the-PIT-Timer/m-p/725492#M9769</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2018-05-28T10:54:10Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777C-Clock source to the PIT Timer</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777C-Clock-source-to-the-PIT-Timer/m-p/725493#M9770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Petr,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Yes, i have gone through&amp;nbsp;&lt;SPAN&gt;startup . And thanks alot for this help.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 May 2018 07:49:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777C-Clock-source-to-the-PIT-Timer/m-p/725493#M9770</guid>
      <dc:creator>yashkumar</dc:creator>
      <dc:date>2018-05-29T07:49:38Z</dc:date>
    </item>
  </channel>
</rss>