<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: Project compiled by S32 2017.R1 is not working with booloader</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Project-compiled-by-S32-2017-R1-is-not-working-with-booloader/m-p/722701#M9681</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Martin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;I've managed to get rid of this problem already, though I'm not quite sure about the real cause. The thing is that I use pit in the bootloader, if I disable pit before jumping to app, then it works fine. But the situation is not the same when I use S32DS v1.1/v1.2. Do you have any idea?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jan 2018 05:44:35 GMT</pubDate>
    <dc:creator>jeromeli</dc:creator>
    <dc:date>2018-01-17T05:44:35Z</dc:date>
    <item>
      <title>Project compiled by S32 2017.R1 is not working with booloader</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Project-compiled-by-S32-2017-R1-is-not-working-with-booloader/m-p/722699#M9679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My&amp;nbsp;project that compiled in S32DS 2017.R1 is not working with my&amp;nbsp;CAN&amp;nbsp;bootloader. While the&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;bootloader is fine with projects that are compiled in S32DS v1.1/v1.2.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCU: MPC5748G&lt;/P&gt;&lt;P&gt;SDK: EAR 0.8.1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestion on how to study the cause of the problem? Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jan 2018 12:11:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Project-compiled-by-S32-2017-R1-is-not-working-with-booloader/m-p/722699#M9679</guid>
      <dc:creator>jeromeli</dc:creator>
      <dc:date>2018-01-15T12:11:28Z</dc:date>
    </item>
    <item>
      <title>Re: Project compiled by S32 2017.R1 is not working with booloader</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Project-compiled-by-S32-2017-R1-is-not-working-with-booloader/m-p/722700#M9680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jerome,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you please specify, what does it mean application is not working? I need to know as much details as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just quick question, do you place anything into custom RAM section?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2018 12:29:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Project-compiled-by-S32-2017-R1-is-not-working-with-booloader/m-p/722700#M9680</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2018-01-16T12:29:01Z</dc:date>
    </item>
    <item>
      <title>Re: Project compiled by S32 2017.R1 is not working with booloader</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Project-compiled-by-S32-2017-R1-is-not-working-with-booloader/m-p/722701#M9681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Martin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;I've managed to get rid of this problem already, though I'm not quite sure about the real cause. The thing is that I use pit in the bootloader, if I disable pit before jumping to app, then it works fine. But the situation is not the same when I use S32DS v1.1/v1.2. Do you have any idea?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 05:44:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Project-compiled-by-S32-2017-R1-is-not-working-with-booloader/m-p/722701#M9681</guid>
      <dc:creator>jeromeli</dc:creator>
      <dc:date>2018-01-17T05:44:35Z</dc:date>
    </item>
    <item>
      <title>Re: Project compiled by S32 2017.R1 is not working with booloader</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Project-compiled-by-S32-2017-R1-is-not-working-with-booloader/m-p/722702#M9682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jerome,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately, I do not have enough information, so I do not have any idea, what could be wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can recommend you some general points.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If your bootloader runs the application directly without microcontroller reset, please ensure that bootloader cleans up all resources which it used.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, you did not explain the behavior. Does it mean that bootloader does not run the application at all, or application does not run correct, or...?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please write me back as much details as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jan 2018 08:54:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Project-compiled-by-S32-2017-R1-is-not-working-with-booloader/m-p/722702#M9682</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2018-01-18T08:54:09Z</dc:date>
    </item>
  </channel>
</rss>