<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic UJA1023 Configuration Questions (Error Message and Data Dump) in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/UJA1023-Configuration-Questions-Error-Message-and-Data-Dump/m-p/719965#M9613</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am looking to configure UJA1023, but data sheet seems to conflict with LIN 2.0 consortium specification in a few areas (see below for detail). Would anyone be able to help clarify how to properly set up LDF file for this hardware?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;1) In example on page 29 of data sheet, PCI of 2 and 4 is used for Data Dump Frames 3 and 4, respectively. I was under the impression that these 0x3C/0x3D frames should always have PCI of 6. What is the proper configuration to use to ensure proper communication between Master and Slave?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;2) During LDF consistency check, I get a warning message that there is missing attribute "reponse_error". However&amp;nbsp;I do not believe I am able to define a response_error signal in LDF since UJA1023 error response signal is only accessible via 0xB4 service ID and is not reported as part of an unconditioned frame.&amp;nbsp;Has anyone else run into this issue?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Apr 2018 12:41:10 GMT</pubDate>
    <dc:creator>mmcneely</dc:creator>
    <dc:date>2018-04-10T12:41:10Z</dc:date>
    <item>
      <title>UJA1023 Configuration Questions (Error Message and Data Dump)</title>
      <link>https://community.nxp.com/t5/MPC5xxx/UJA1023-Configuration-Questions-Error-Message-and-Data-Dump/m-p/719965#M9613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am looking to configure UJA1023, but data sheet seems to conflict with LIN 2.0 consortium specification in a few areas (see below for detail). Would anyone be able to help clarify how to properly set up LDF file for this hardware?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;1) In example on page 29 of data sheet, PCI of 2 and 4 is used for Data Dump Frames 3 and 4, respectively. I was under the impression that these 0x3C/0x3D frames should always have PCI of 6. What is the proper configuration to use to ensure proper communication between Master and Slave?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;2) During LDF consistency check, I get a warning message that there is missing attribute "reponse_error". However&amp;nbsp;I do not believe I am able to define a response_error signal in LDF since UJA1023 error response signal is only accessible via 0xB4 service ID and is not reported as part of an unconditioned frame.&amp;nbsp;Has anyone else run into this issue?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2018 12:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/UJA1023-Configuration-Questions-Error-Message-and-Data-Dump/m-p/719965#M9613</guid>
      <dc:creator>mmcneely</dc:creator>
      <dc:date>2018-04-10T12:41:10Z</dc:date>
    </item>
  </channel>
</rss>