<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to upload multiple elf to MPC5674F? in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/How-to-upload-multiple-elf-to-MPC5674F/m-p/719491#M9599</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi~~&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our project should divide the following executable files(elf) for certification:&lt;BR /&gt;- one of elf performs the function of the bootloader.&lt;BR /&gt;- one of elf performs the main functions.&lt;BR /&gt;- one of elf stores data into external memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have encountered the following problems during developing the project using Code Warrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. I will upload two or more executable files to one target board. How do i modify the supplied lcf file and startup code (MPC5674F based).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. I use the ICDPPCNEXUS debugger included our code warrior package. I want to upload multi executable files to the target board using the this debugger. when i use this debugger, it seems that the previously uploaded elf file is deleted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. I want to jump from the A project to the start point of B project. How do i use assembler? Thank you for your example. (The bl command was executed but i was failed)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Nov 2017 00:45:25 GMT</pubDate>
    <dc:creator>chunghohwang</dc:creator>
    <dc:date>2017-11-20T00:45:25Z</dc:date>
    <item>
      <title>How to upload multiple elf to MPC5674F?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/How-to-upload-multiple-elf-to-MPC5674F/m-p/719491#M9599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi~~&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our project should divide the following executable files(elf) for certification:&lt;BR /&gt;- one of elf performs the function of the bootloader.&lt;BR /&gt;- one of elf performs the main functions.&lt;BR /&gt;- one of elf stores data into external memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have encountered the following problems during developing the project using Code Warrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. I will upload two or more executable files to one target board. How do i modify the supplied lcf file and startup code (MPC5674F based).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. I use the ICDPPCNEXUS debugger included our code warrior package. I want to upload multi executable files to the target board using the this debugger. when i use this debugger, it seems that the previously uploaded elf file is deleted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. I want to jump from the A project to the start point of B project. How do i use assembler? Thank you for your example. (The bl command was executed but i was failed)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Nov 2017 00:45:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/How-to-upload-multiple-elf-to-MPC5674F/m-p/719491#M9599</guid>
      <dc:creator>chunghohwang</dc:creator>
      <dc:date>2017-11-20T00:45:25Z</dc:date>
    </item>
  </channel>
</rss>