<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: Question about Leopard MPC5643L</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Question-about-Leopard-MPC5643L/m-p/423578#M955</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;During and after reset almost all GPIO pins are in high-z state, until you configure the PCR registers, for example weak pull-down/up etc. &lt;/P&gt;&lt;P&gt;The PWM module control the output once the PA field in PCR register is set for PWM function and when PWM.OUTEN register&amp;nbsp; is configured. In that case the polarity of the PWM output is done by PWM.SUBx.OCTRL[POLx] bits.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 May 2015 14:09:12 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2015-05-12T14:09:12Z</dc:date>
    <item>
      <title>Question about Leopard MPC5643L</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Question-about-Leopard-MPC5643L/m-p/423577#M954</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;H4&gt;Hi guys,&lt;/H4&gt;&lt;H4&gt;&lt;/H4&gt;&lt;H4&gt;I have a problem when I program my MPC5643L and is that all the DIOS get high level. I have two PWM that control two valves and when I program the MCU, the PWMs are activated. Any one knows if exist any configuration option to avoid this issue. I am working now in changing &lt;SPAN style="font-weight: bold; color: #6a6a6a; font-family: arial, sans-serif; font-size: small;"&gt;hardwardly the polarity of the signal, but this will be my last chance.&lt;/SPAN&gt;&lt;/H4&gt;&lt;H4&gt;&lt;/H4&gt;&lt;H4&gt;Any idea. Thanks in advance&lt;/H4&gt;&lt;H4&gt;&lt;/H4&gt;&lt;H4&gt;Best regards&lt;/H4&gt;&lt;H4&gt;&lt;/H4&gt;&lt;H4&gt;Pablo &lt;/H4&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2015 10:18:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Question-about-Leopard-MPC5643L/m-p/423577#M954</guid>
      <dc:creator>pabloprieto</dc:creator>
      <dc:date>2015-05-12T10:18:06Z</dc:date>
    </item>
    <item>
      <title>Re: Question about Leopard MPC5643L</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Question-about-Leopard-MPC5643L/m-p/423578#M955</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;During and after reset almost all GPIO pins are in high-z state, until you configure the PCR registers, for example weak pull-down/up etc. &lt;/P&gt;&lt;P&gt;The PWM module control the output once the PA field in PCR register is set for PWM function and when PWM.OUTEN register&amp;nbsp; is configured. In that case the polarity of the PWM output is done by PWM.SUBx.OCTRL[POLx] bits.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2015 14:09:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Question-about-Leopard-MPC5643L/m-p/423578#M955</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2015-05-12T14:09:12Z</dc:date>
    </item>
    <item>
      <title>Re: Question about Leopard MPC5643L</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Question-about-Leopard-MPC5643L/m-p/423579#M956</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will try with a pull down.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pablo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2015 14:55:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Question-about-Leopard-MPC5643L/m-p/423579#M956</guid>
      <dc:creator>pabloprieto</dc:creator>
      <dc:date>2015-05-12T14:55:52Z</dc:date>
    </item>
    <item>
      <title>Re: Question about Leopard MPC5643L</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Question-about-Leopard-MPC5643L/m-p/423580#M957</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you sure that &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;During and after reset almost all GPIO pins are in high-z state, because I'm trying with a pull down and it is not working, I always obtain high level.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pablo &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2015 07:34:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Question-about-Leopard-MPC5643L/m-p/423580#M957</guid>
      <dc:creator>pabloprieto</dc:creator>
      <dc:date>2015-05-13T07:34:21Z</dc:date>
    </item>
    <item>
      <title>Re: Question about Leopard MPC5643L</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Question-about-Leopard-MPC5643L/m-p/423581#M958</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pablo, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The state of the pin can be checked against a Pin summary table of the device Reference manual (chapter 3.4; &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/ref_manual/MPC5643LRM.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/MPC5643LRM.pdf&lt;/A&gt;&lt;SPAN&gt;) and/or SIUL PCR register description (chapter 47.5.2.8).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Maybe the external circuitry connected to the pin pulls it high and weak internal pull-down is not enough to hold it down.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2015 09:58:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Question-about-Leopard-MPC5643L/m-p/423581#M958</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2015-05-13T09:58:28Z</dc:date>
    </item>
    <item>
      <title>Re: Question about Leopard MPC5643L</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Question-about-Leopard-MPC5643L/m-p/423582#M959</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petrs,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have solved the problem. We were using very weak pull down. Now with an stronger one, it works perfectly, thank you very much for your support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pablo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2015 10:31:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Question-about-Leopard-MPC5643L/m-p/423582#M959</guid>
      <dc:creator>pabloprieto</dc:creator>
      <dc:date>2015-05-13T10:31:33Z</dc:date>
    </item>
  </channel>
</rss>