<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: JTAG censorship in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/JTAG-censorship/m-p/716062#M9529</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am still unable to uncensor the device through JTAG.&amp;nbsp; Maybe my timings are not good.&amp;nbsp; At which point the password entered through JTAG is compared with the one strored in memory.&amp;nbsp; Is is right after reset is released???&amp;nbsp; At which point in time this comparison takes place???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 31 Aug 2018 18:53:09 GMT</pubDate>
    <dc:creator>vincentbbbb</dc:creator>
    <dc:date>2018-08-31T18:53:09Z</dc:date>
    <item>
      <title>JTAG censorship</title>
      <link>https://community.nxp.com/t5/MPC5xxx/JTAG-censorship/m-p/716060#M9527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using my own JTAG programmer and I was having difficulty inputting JTAG censorship value for my MPC5674F.&amp;nbsp; I am able to read memory of an uncensored device, but when I put a censorship value, I am not able to read the memory.&amp;nbsp; I was wondering at what moment the censorship data was compared to the one in Flash???&amp;nbsp; Is it right after it is sent via JTAG or is it when requesting a read command??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 May 2018 12:51:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/JTAG-censorship/m-p/716060#M9527</guid>
      <dc:creator>vincentbbbb</dc:creator>
      <dc:date>2018-05-01T12:51:17Z</dc:date>
    </item>
    <item>
      <title>Re: JTAG censorship</title>
      <link>https://community.nxp.com/t5/MPC5xxx/JTAG-censorship/m-p/716061#M9528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, please pay attention to sections&lt;/P&gt;&lt;P&gt;8.5.7 Enabling Debug of a Censored Device and&lt;/P&gt;&lt;P&gt;31.3.4 CENSOR_CTRL Register&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;of device's RM:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/reference-manual/MPC5674FRM.pdf" title="https://www.nxp.com/docs/en/reference-manual/MPC5674FRM.pdf"&gt;https://www.nxp.com/docs/en/reference-manual/MPC5674FRM.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using your own debugger, I believe these chapters are understandable to you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I could also point out following appnote:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN4365.pdf" title="https://www.nxp.com/docs/en/application-note/AN4365.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN4365.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps a bit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 May 2018 15:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/JTAG-censorship/m-p/716061#M9528</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2018-05-03T15:18:56Z</dc:date>
    </item>
    <item>
      <title>Re: JTAG censorship</title>
      <link>https://community.nxp.com/t5/MPC5xxx/JTAG-censorship/m-p/716062#M9529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am still unable to uncensor the device through JTAG.&amp;nbsp; Maybe my timings are not good.&amp;nbsp; At which point the password entered through JTAG is compared with the one strored in memory.&amp;nbsp; Is is right after reset is released???&amp;nbsp; At which point in time this comparison takes place???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Aug 2018 18:53:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/JTAG-censorship/m-p/716062#M9529</guid>
      <dc:creator>vincentbbbb</dc:creator>
      <dc:date>2018-08-31T18:53:09Z</dc:date>
    </item>
    <item>
      <title>Re: JTAG censorship</title>
      <link>https://community.nxp.com/t5/MPC5xxx/JTAG-censorship/m-p/716063#M9530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;JTAG censorship is compared during reset phase.&lt;/P&gt;&lt;P&gt;Once you send the correct password the JTAG module will start communicating. Until then it behaves as there is no JTAG module on chip to external world.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2019 11:09:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/JTAG-censorship/m-p/716063#M9530</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2019-07-16T11:09:41Z</dc:date>
    </item>
    <item>
      <title>Re: JTAG censorship</title>
      <link>https://community.nxp.com/t5/MPC5xxx/JTAG-censorship/m-p/2110263#M27690</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello, my program is in Flash. I placed the demo program in the initialization of my program, but as a result, neither my boot nor my APP can start.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jun 2025 09:00:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/JTAG-censorship/m-p/2110263#M27690</guid>
      <dc:creator>Jia_Jun_LI</dc:creator>
      <dc:date>2025-06-04T09:00:17Z</dc:date>
    </item>
  </channel>
</rss>