<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Doubt about using SIUL2 on MPC5777M in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Doubt-about-using-SIUL2-on-MPC5777M/m-p/714259#M9435</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrea,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can simply refer to TSENS example posted here: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-334438"&gt;https://community.nxp.com/docs/DOC-334438&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the reading of ADC internal channels you do not need to set SIUL&lt;/P&gt;&lt;P&gt;To configure other GPIO pins (UART, etc) you should refer to I/O Signal Description and Input Multiplexing table, which is normally attached within a device Reference Manual. It is missing in the latest rev.4.3. You can find it e.g. here &lt;A _jive_internal="true" href="https://community.nxp.com/message/890202"&gt;https://community.nxp.com/message/890202&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Sep 2017 05:07:49 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2017-09-04T05:07:49Z</dc:date>
    <item>
      <title>Doubt about using SIUL2 on MPC5777M</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Doubt-about-using-SIUL2-on-MPC5777M/m-p/714258#M9434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello to all,&lt;/P&gt;&lt;P&gt;I'm working with the MPC5777M. I'm trying to convert the temperature using SAR_ADC_B0 and then send the value via UART, also using INTC (interrput controller) and PIT (timer)&lt;/P&gt;&lt;P&gt;It is unclear if and how to configure the SIUL module. I've seen some examples of configuring this module, but I do not know where to find the information in the manual to configure it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding the SAR_ADC_B0 I just need to convert PTAT and CTAT channels (channel 120 and 121). To do this, do i&amp;nbsp;need to configure SIUL? And what about UART? Can anyone help me to clarify the ideas?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Sep 2017 16:22:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Doubt-about-using-SIUL2-on-MPC5777M/m-p/714258#M9434</guid>
      <dc:creator>andrerm</dc:creator>
      <dc:date>2017-09-03T16:22:15Z</dc:date>
    </item>
    <item>
      <title>Re: Doubt about using SIUL2 on MPC5777M</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Doubt-about-using-SIUL2-on-MPC5777M/m-p/714259#M9435</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrea,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can simply refer to TSENS example posted here: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-334438"&gt;https://community.nxp.com/docs/DOC-334438&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the reading of ADC internal channels you do not need to set SIUL&lt;/P&gt;&lt;P&gt;To configure other GPIO pins (UART, etc) you should refer to I/O Signal Description and Input Multiplexing table, which is normally attached within a device Reference Manual. It is missing in the latest rev.4.3. You can find it e.g. here &lt;A _jive_internal="true" href="https://community.nxp.com/message/890202"&gt;https://community.nxp.com/message/890202&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Sep 2017 05:07:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Doubt-about-using-SIUL2-on-MPC5777M/m-p/714259#M9435</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-09-04T05:07:49Z</dc:date>
    </item>
  </channel>
</rss>