<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flash Error Injection methods on MPC5674F in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Flash-Error-Injection-methods-on-MPC5674F/m-p/712856#M9366</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I solved this problem with your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Sep 2017 11:21:39 GMT</pubDate>
    <dc:creator>youngseolee</dc:creator>
    <dc:date>2017-09-26T11:21:39Z</dc:date>
    <item>
      <title>Flash Error Injection methods on MPC5674F</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flash-Error-Injection-methods-on-MPC5674F/m-p/712852#M9362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi threre,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have a question about Flash error injection methods on MPC5674F.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in the reference menual of MPC5674F, a ECSM(error correction status module) do not support Flash error injection bits.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need the flash error injection function, is there any way I can do it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please answer,&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2017 00:21:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flash-Error-Injection-methods-on-MPC5674F/m-p/712852#M9362</guid>
      <dc:creator>youngseolee</dc:creator>
      <dc:date>2017-09-26T00:21:56Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Error Injection methods on MPC5674F</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flash-Error-Injection-methods-on-MPC5674F/m-p/712853#M9363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, it can be done by flash over-programming. Pay attention to AN5200, section 5.2:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-103300"&gt;AN5200 - Error Correcting Codes Implemented on MPC55xx and MPC56xx&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and its example 4 or 5:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-102012"&gt;Example MPC5643L 2b RAM and 2b FLASH ECC error injection CW210&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105443"&gt;https://community.nxp.com/docs/DOC-105443&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or you may see following one:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-332668"&gt;Example MPC5777C-1b+2b_FLASH_ECC_error_injection GHS614&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2017 08:37:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flash-Error-Injection-methods-on-MPC5674F/m-p/712853#M9363</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2017-09-26T08:37:34Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Error Injection methods on MPC5674F</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flash-Error-Injection-methods-on-MPC5674F/m-p/712854#M9364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, david&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I&amp;nbsp;have been implemented a non-correctable error injection code on the MPC5675F with reference to the AN5200 and the MPC5674K example code.&lt;/P&gt;&lt;P&gt;also, i am trying to implement an 1bit error injection code, but an 1bit&amp;nbsp;error reporting interrupt does not occur.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My program sequence is as follows.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. write the original data A(0x0000000000000001) to a flash memory location (Flash_B: 0x00EFC008 ~ C).&lt;/P&gt;&lt;P&gt;2. Over program data A to data B(0x0000000000000002) to the same flash memory location.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can not inject 1bit errors in this way? or&amp;nbsp;Is the combination of input data A / B wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2017 10:58:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flash-Error-Injection-methods-on-MPC5674F/m-p/712854#M9364</guid>
      <dc:creator>youngseolee</dc:creator>
      <dc:date>2017-09-26T10:58:07Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Error Injection methods on MPC5674F</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flash-Error-Injection-methods-on-MPC5674F/m-p/712855#M9365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Single bit ECC error reporting must be also enabled in UT0[SCBE]. Following sequence must be used for that:&lt;/P&gt;&lt;P&gt;/* 1. Enable UTest mode */&lt;BR /&gt;CFLASH.UT0.R = 0xF9F99999;&lt;BR /&gt;/* 2. Enable single bit error correction */&lt;BR /&gt;CFLASH.UT0.B.SBCE = 1;&lt;BR /&gt;/* 3. Finish the UTest mode by writing UT0[UTE] with 0. */&lt;BR /&gt;CFLASH.UT0.B.UTE = 0;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;Chosen pattern for single bit injection may be as follows:&lt;/P&gt;&lt;P class=""&gt;1. Write the original data A = 0xFFFFFFFF00000000 (syndrome X) to a flash memory location.&lt;/P&gt;&lt;P class=""&gt;2. Over program data A to data B = 0xFFFFFFFF00000001 (syndrome Y) to the same flash memory location.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2017 11:04:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flash-Error-Injection-methods-on-MPC5674F/m-p/712855#M9365</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2017-09-26T11:04:56Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Error Injection methods on MPC5674F</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flash-Error-Injection-methods-on-MPC5674F/m-p/712856#M9366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I solved this problem with your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2017 11:21:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flash-Error-Injection-methods-on-MPC5674F/m-p/712856#M9366</guid>
      <dc:creator>youngseolee</dc:creator>
      <dc:date>2017-09-26T11:21:39Z</dc:date>
    </item>
  </channel>
</rss>