<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックEEPROM Emulation</title>
    <link>https://community.nxp.com/t5/MPC5xxx/EEPROM-Emulation/m-p/712251#M9342</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I want to do EEPROM emulation on MPC5602P.I had gone through the &lt;A href="https://www.nxp.com/docs/en/application-note/AN4868.pdf"&gt;&lt;SPAN style="color: #0066cc; text-decoration: underline;"&gt;AN4868&lt;/SPAN&gt;&lt;/A&gt; and I tried to implement it on my CodeWarrior platform.&amp;nbsp;And I got EEE_Driver_v1.3.0 and I installed it, which had demo project for MPC5604P.&amp;nbsp;I understood a bit, I just have to fill the data in buffer and then the write and read operations&amp;nbsp;should be done&amp;nbsp;as mentioned in the main file. &amp;nbsp;As per the &lt;A _jive_internal="true" href="https://community.nxp.com/thread/392009"&gt;&lt;SPAN style="color: #0066cc; text-decoration: underline;"&gt;suggestion from the post,&lt;/SPAN&gt;&lt;/A&gt;&amp;nbsp;I modified the settings. I tried flashing to my MPC5602P.&amp;nbsp;Also I created a new project (attached here) and imported all the related files tried to flash it. But my code got stuck in&amp;nbsp; main() -&amp;gt; "Write eeprom data records".&amp;nbsp;FSL_&lt;STRONG&gt;WriteEeprom&lt;/STRONG&gt; is returning 0x0020, which is &lt;SPAN style="font-size: medium;"&gt;EE_ERROR_MISMATCH&lt;/SPAN&gt;, so it always stuck in that while(stop_flag).&lt;/P&gt;&lt;P&gt;Do I need to modify .lcf file to make it work. If yes try which part I need to edit. Looking forward to see some help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Rajendranath&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 Oct 2017 11:14:52 GMT</pubDate>
    <dc:creator>bjrajendra</dc:creator>
    <dc:date>2017-10-21T11:14:52Z</dc:date>
    <item>
      <title>EEPROM Emulation</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EEPROM-Emulation/m-p/712251#M9342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I want to do EEPROM emulation on MPC5602P.I had gone through the &lt;A href="https://www.nxp.com/docs/en/application-note/AN4868.pdf"&gt;&lt;SPAN style="color: #0066cc; text-decoration: underline;"&gt;AN4868&lt;/SPAN&gt;&lt;/A&gt; and I tried to implement it on my CodeWarrior platform.&amp;nbsp;And I got EEE_Driver_v1.3.0 and I installed it, which had demo project for MPC5604P.&amp;nbsp;I understood a bit, I just have to fill the data in buffer and then the write and read operations&amp;nbsp;should be done&amp;nbsp;as mentioned in the main file. &amp;nbsp;As per the &lt;A _jive_internal="true" href="https://community.nxp.com/thread/392009"&gt;&lt;SPAN style="color: #0066cc; text-decoration: underline;"&gt;suggestion from the post,&lt;/SPAN&gt;&lt;/A&gt;&amp;nbsp;I modified the settings. I tried flashing to my MPC5602P.&amp;nbsp;Also I created a new project (attached here) and imported all the related files tried to flash it. But my code got stuck in&amp;nbsp; main() -&amp;gt; "Write eeprom data records".&amp;nbsp;FSL_&lt;STRONG&gt;WriteEeprom&lt;/STRONG&gt; is returning 0x0020, which is &lt;SPAN style="font-size: medium;"&gt;EE_ERROR_MISMATCH&lt;/SPAN&gt;, so it always stuck in that while(stop_flag).&lt;/P&gt;&lt;P&gt;Do I need to modify .lcf file to make it work. If yes try which part I need to edit. Looking forward to see some help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Rajendranath&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Oct 2017 11:14:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EEPROM-Emulation/m-p/712251#M9342</guid>
      <dc:creator>bjrajendra</dc:creator>
      <dc:date>2017-10-21T11:14:52Z</dc:date>
    </item>
  </channel>
</rss>