<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 56xx SWT Configuration in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/56xx-SWT-Configuration/m-p/711806#M9326</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is because the debugger by default disable SWT.&lt;/P&gt;&lt;P&gt;Enable it in debug options of debugger or run your code wihtout debugger at all.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Oct 2017 10:23:30 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2017-10-20T10:23:30Z</dc:date>
    <item>
      <title>56xx SWT Configuration</title>
      <link>https://community.nxp.com/t5/MPC5xxx/56xx-SWT-Configuration/m-p/711805#M9325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can anyone suggest a reason&amp;nbsp;as to what's wrong with this attempt to configure the SWT on a 56xx device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On entry to the code SWT.CR.R = 0xFF00010A - so watchdog is disabled and SLK is cleared.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define SWT_UNLOCK1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xC520&lt;BR /&gt;#define SWT_UNLOCK2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xD928&lt;BR /&gt;#define SWT_5MSTIMEOUT&amp;nbsp;&amp;nbsp; 0x13880&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* 16MHz Internal &lt;A href="mailto:osc..@5ms"&gt;osc..@5ms&lt;/A&gt; timeout =&amp;gt; 16MHz/200 = 80000 = 0x13880 */&lt;BR /&gt;#define SWT_SLK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000010&amp;nbsp; /* Mask for software lock bit */&lt;BR /&gt;#define SWT_WEN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000001&amp;nbsp; /* Mask for watchdog enable bit */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;/* Routine to setup software watchdog timer */&lt;BR /&gt;&amp;nbsp;/* If watchdog is disabled - set it up, otherwise leave it alone */&lt;BR /&gt;&amp;nbsp;if (!(SWT.CR.R &amp;amp; SWT_WEN))&lt;BR /&gt;&amp;nbsp;{&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (SWT.CR.R &amp;amp; SWT_SLK)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Soft lock bit is on - unlock the control register */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Unlock the control register */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SWT.SR.R = SWT_UNLOCK1;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SWT.SR.R = SWT_UNLOCK2;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*&amp;nbsp; Wait here for SLK to clear */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while(SWT.CR.R &amp;amp; SWT_SLK);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* CR should now be writable&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SWT.CR.R |= SWT_WEN;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Set timeout interval */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SWT.TO.R = SWT_5MSTIMEOUT;&lt;BR /&gt;&amp;nbsp;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On exit of this code, the SWT.TO register has been updated, but no matter what I do to write to SWT.CR (including, for instance SWT.CR.R = 0xFF00010B;) the watchdog remains disabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea why this is?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any suggestions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Oct 2017 09:46:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/56xx-SWT-Configuration/m-p/711805#M9325</guid>
      <dc:creator>aero72</dc:creator>
      <dc:date>2017-10-20T09:46:22Z</dc:date>
    </item>
    <item>
      <title>Re: 56xx SWT Configuration</title>
      <link>https://community.nxp.com/t5/MPC5xxx/56xx-SWT-Configuration/m-p/711806#M9326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is because the debugger by default disable SWT.&lt;/P&gt;&lt;P&gt;Enable it in debug options of debugger or run your code wihtout debugger at all.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Oct 2017 10:23:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/56xx-SWT-Configuration/m-p/711806#M9326</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-10-20T10:23:30Z</dc:date>
    </item>
  </channel>
</rss>