<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to access test flash memory in MPC5643L? in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/How-to-access-test-flash-memory-in-MPC5643L/m-p/709075#M9172</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you see following example, in the main function you see how to access test flash&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-101714"&gt;Example MPC5643L TSENS Temperature_calculation CW210&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Access with READ_FROM_TF macro I have tried as well and I can give you a example if you want, but it is not recommended procedure.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Oct 2017 13:59:11 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2017-10-17T13:59:11Z</dc:date>
    <item>
      <title>How to access test flash memory in MPC5643L?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/How-to-access-test-flash-memory-in-MPC5643L/m-p/709074#M9171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Could anyone help me to access the test flash memory in MPC5643L?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to configure the self test analog watchdog register for ADC for which the calibration values are available in test flash memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried the macro "READ_FROM_TF" from the "MPC5643L.h" file with below code. But the macro has not executed successfully, instead the application goes to unknown location.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static uint32 ReadFromTestFlash(void)&lt;BR /&gt;{&lt;BR /&gt; uint32 RetVal, SysStatus1, SysStatus2;&lt;BR /&gt;SysStatus1 = *((uint32*)(0xC3FD8000UL ));&lt;BR /&gt; //Set TFE bit &lt;BR /&gt; *((uint32*)(0xC3FD8000UL + 0x0024UL)) |= 0x00000004UL;&lt;BR /&gt; SysStatus2 = *((uint32*)(0xC3FD8000UL + 0x0024UL));&lt;BR /&gt; READ_FROM_TF(&amp;amp;TestFalshBuf[0], RetVal);&lt;BR /&gt; //Reset TFE bit&lt;BR /&gt; *((uint32*)(0xC3FD8000UL + 0x0024UL)) &amp;amp;= ~0x00000004UL;&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Oct 2017 12:17:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/How-to-access-test-flash-memory-in-MPC5643L/m-p/709074#M9171</guid>
      <dc:creator>rajakumaranazha</dc:creator>
      <dc:date>2017-10-17T12:17:17Z</dc:date>
    </item>
    <item>
      <title>Re: How to access test flash memory in MPC5643L?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/How-to-access-test-flash-memory-in-MPC5643L/m-p/709075#M9172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you see following example, in the main function you see how to access test flash&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-101714"&gt;Example MPC5643L TSENS Temperature_calculation CW210&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Access with READ_FROM_TF macro I have tried as well and I can give you a example if you want, but it is not recommended procedure.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Oct 2017 13:59:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/How-to-access-test-flash-memory-in-MPC5643L/m-p/709075#M9172</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2017-10-17T13:59:11Z</dc:date>
    </item>
  </channel>
</rss>