<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: Diffrence between SCI and eSCI</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Diffrence-between-SCI-and-eSCI/m-p/417495#M905</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Quoting Wikipedia:&lt;/P&gt;&lt;P&gt;'The term "Serial Communications Interface" (SCI) was first used at Motorola around 1975 to refer to their start-stop asynchronous serial interface device, which others were calling a UART. '&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The terms SCI and UART are synonyms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our specific module implementation eSCI, used on certain MPC56xx devices, offers 2 functionalities: UART and LIN. &lt;/P&gt;&lt;P&gt;Note that LinFlex module that is being used on the rest of MPC56xx is the different module (coming from JDP program), however offers the same functionalities (UART and LIN).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Simple example code you may find here, chapter 15 and 16:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN2865.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN2865.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Jun 2015 11:32:29 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2015-06-22T11:32:29Z</dc:date>
    <item>
      <title>Diffrence between SCI and eSCI</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Diffrence-between-SCI-and-eSCI/m-p/417494#M904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi friend,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Kindly give me the diffrence between SCI and eSCI in MPc5674F. and also give one sample code &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2015 07:00:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Diffrence-between-SCI-and-eSCI/m-p/417494#M904</guid>
      <dc:creator>rajiilangovan</dc:creator>
      <dc:date>2015-06-22T07:00:59Z</dc:date>
    </item>
    <item>
      <title>Re: Diffrence between SCI and eSCI</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Diffrence-between-SCI-and-eSCI/m-p/417495#M905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Quoting Wikipedia:&lt;/P&gt;&lt;P&gt;'The term "Serial Communications Interface" (SCI) was first used at Motorola around 1975 to refer to their start-stop asynchronous serial interface device, which others were calling a UART. '&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The terms SCI and UART are synonyms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our specific module implementation eSCI, used on certain MPC56xx devices, offers 2 functionalities: UART and LIN. &lt;/P&gt;&lt;P&gt;Note that LinFlex module that is being used on the rest of MPC56xx is the different module (coming from JDP program), however offers the same functionalities (UART and LIN).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Simple example code you may find here, chapter 15 and 16:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN2865.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN2865.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2015 11:32:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Diffrence-between-SCI-and-eSCI/m-p/417495#M905</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2015-06-22T11:32:29Z</dc:date>
    </item>
  </channel>
</rss>