<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 MPC5746R I/O initial</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-I-O-initial/m-p/701055#M8835</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I found there are 2 kinds of input can be configured for MPC5746R PJ[14]: DSPI0 clock input and error input for FCCU. Please see attachment. But i can't find how to distinguish them. Can you help check which register can be set to enable/disable each module? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Oct 2017 06:45:15 GMT</pubDate>
    <dc:creator>BoxLi</dc:creator>
    <dc:date>2017-10-09T06:45:15Z</dc:date>
    <item>
      <title>MPC5746R I/O initial</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-I-O-initial/m-p/701055#M8835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I found there are 2 kinds of input can be configured for MPC5746R PJ[14]: DSPI0 clock input and error input for FCCU. Please see attachment. But i can't find how to distinguish them. Can you help check which register can be set to enable/disable each module? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Oct 2017 06:45:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5746R-I-O-initial/m-p/701055#M8835</guid>
      <dc:creator>BoxLi</dc:creator>
      <dc:date>2017-10-09T06:45:15Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5746R I/O initial</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-I-O-initial/m-p/701056#M8836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;They are both connected on input of PJ[14].&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Oct 2017 11:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5746R-I-O-initial/m-p/701056#M8836</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-10-09T11:33:56Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5746R I/O initial</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-I-O-initial/m-p/701057#M8837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Peter Vlna wrote:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;They are both connected on input of PJ[14].&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Hi Peter:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Do you mean that the input signal of PJ[14] connect to DSPI and FCCU module simultaneous(seting PAD158 input)? Thanks.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Oct 2017 01:06:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5746R-I-O-initial/m-p/701057#M8837</guid>
      <dc:creator>BoxLi</dc:creator>
      <dc:date>2017-10-10T01:06:03Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5746R I/O initial</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-I-O-initial/m-p/701058#M8838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes,&lt;/P&gt;&lt;P&gt;This is what I expect.&lt;/P&gt;&lt;P&gt;However there can be conflict which I am right now discussing with design.&lt;/P&gt;&lt;P&gt;In scenario where you have PJ[14] selected as input and SPI clock is as input on this pin the FCCU NCF[60] will be set.&lt;/P&gt;&lt;P&gt;On other device (MPC5748G) there is separated IMCR for FCCU[ERRIN] and DSPI. So user can select the input functionality. However here is not this possibility according to IO table.&lt;/P&gt;&lt;P&gt;I will update you when design say they statement.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Oct 2017 07:52:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5746R-I-O-initial/m-p/701058#M8838</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-10-10T07:52:18Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5746R I/O initial</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-I-O-initial/m-p/701059#M8839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Any update on this issue? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Oct 2017 03:59:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5746R-I-O-initial/m-p/701059#M8839</guid>
      <dc:creator>BoxLi</dc:creator>
      <dc:date>2017-10-16T03:59:15Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5746R I/O initial</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-I-O-initial/m-p/701060#M8840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;No, still no answer from application/design team.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Oct 2017 13:13:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5746R-I-O-initial/m-p/701060#M8840</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-10-16T13:13:03Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5746R I/O initial</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-I-O-initial/m-p/701061#M8841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This issue is clear now.&lt;/P&gt;&lt;P&gt;The DSPI CLKIN and FCCU ERRIN are both rooted as input without possibility to select or disable one of them.&lt;/P&gt;&lt;P&gt;Therefore when DPSI clock input is on pin PJ[14] user must disable FCCU NCF[60] in FCCU_NCF_E1 register.&lt;/P&gt;&lt;P&gt;However this will still rise fault NCF[60] in FCCU_NCF_S1.&lt;/P&gt;&lt;P&gt;If the user SW validate NCF then NCF[60] must be ignored as it is caused by dual input rooting on PJ[14].&lt;/P&gt;&lt;P&gt;User must select either to have DSPI clk in or FCCU ERRIN functionality on this pin.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Nov 2017 12:26:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5746R-I-O-initial/m-p/701061#M8841</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-11-30T12:26:46Z</dc:date>
    </item>
  </channel>
</rss>