<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ECC injection on MPC5746C in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/ECC-injection-on-MPC5746C/m-p/699695#M8779</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have just created example code based on approach I have already described in the link mentioned by you:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-335206"&gt;Example MPC5744P 1b+2b_RAM_ECC_error_injection GHS714&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This approach could be possible to use for RAM error injection on MPC5746C. Flash errors does not need to be injected as there are prepared faulty patterns in UTEST area. Error injection module is not present on MPC5746C device.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Aug 2017 12:38:37 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2017-08-23T12:38:37Z</dc:date>
    <item>
      <title>ECC injection on MPC5746C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/ECC-injection-on-MPC5746C/m-p/699692#M8776</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am developing ECC feature on MPC5744C and getting confusion when trying to create a ECC fake fault (ECC injection) for testing.&lt;/P&gt;&lt;P&gt;At &lt;A _jive_internal="true" href="https://community.nxp.com/thread/450864"&gt;here&lt;/A&gt;, &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/davidtosenovjan"&gt;davidtosenovjan&lt;/A&gt;‌ suggested that can inject via EIM but I couldn't found the same module in MPC5746C. My question is:&lt;/P&gt;&lt;P&gt;- Is there EIM module supported on MPC5746C chip?&lt;/P&gt;&lt;P&gt;- If EIM was not supported, Are there any alternative way to inject ECC on this chip?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Tung Dao.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Aug 2017 04:50:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/ECC-injection-on-MPC5746C/m-p/699692#M8776</guid>
      <dc:creator>ddt_1793</dc:creator>
      <dc:date>2017-08-16T04:50:35Z</dc:date>
    </item>
    <item>
      <title>Re: ECC injection on MPC5746C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/ECC-injection-on-MPC5746C/m-p/699693#M8777</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you have&amp;nbsp;&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;IO_Signal_Description_and_Input_multiplexing_tables.xls about MPC5746C ?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Aug 2017 07:19:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/ECC-injection-on-MPC5746C/m-p/699693#M8777</guid>
      <dc:creator>木子李</dc:creator>
      <dc:date>2017-08-17T07:19:49Z</dc:date>
    </item>
    <item>
      <title>Re: ECC injection on MPC5746C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/ECC-injection-on-MPC5746C/m-p/699694#M8778</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes I have, I have "MPC5746C Reference Manual" which was attached "&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;IO_Signal_Description_and_Input_multiplexing_tables.xls".&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;Which is information you want in that sheet?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Aug 2017 08:43:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/ECC-injection-on-MPC5746C/m-p/699694#M8778</guid>
      <dc:creator>ddt_1793</dc:creator>
      <dc:date>2017-08-17T08:43:28Z</dc:date>
    </item>
    <item>
      <title>Re: ECC injection on MPC5746C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/ECC-injection-on-MPC5746C/m-p/699695#M8779</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have just created example code based on approach I have already described in the link mentioned by you:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-335206"&gt;Example MPC5744P 1b+2b_RAM_ECC_error_injection GHS714&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This approach could be possible to use for RAM error injection on MPC5746C. Flash errors does not need to be injected as there are prepared faulty patterns in UTEST area. Error injection module is not present on MPC5746C device.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Aug 2017 12:38:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/ECC-injection-on-MPC5746C/m-p/699695#M8779</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2017-08-23T12:38:37Z</dc:date>
    </item>
    <item>
      <title>Re: ECC injection on MPC5746C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/ECC-injection-on-MPC5746C/m-p/699696#M8780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the example.&lt;/P&gt;&lt;P&gt;As your code, Which address will getting corruption? Is it possible to change the corrupted address and where?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for you support.&lt;/P&gt;&lt;P&gt;Tung Dao.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Aug 2017 14:32:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/ECC-injection-on-MPC5746C/m-p/699696#M8780</guid>
      <dc:creator>ddt_1793</dc:creator>
      <dc:date>2017-08-23T14:32:55Z</dc:date>
    </item>
  </channel>
</rss>