<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: Protect the code</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Protect-the-code/m-p/698125#M8731</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I expect that you are talking about code encryption.&lt;/P&gt;&lt;P&gt;Unfortunately micro you have chosen does not support HW protection&amp;nbsp; like HSM (hardware security module) or CSE (cryptographic service engine).&lt;/P&gt;&lt;P&gt;On the other hand you can use Flash array integrity check to prevent any unintended code change. But one with source code can easily find and modify the code to skip this check.&lt;/P&gt;&lt;P&gt;It is common that customers use external cryptographic tools to encrypt generated binary output files. This is based on polynomial encrypting and it's quite hard to break these encryption tools.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Aug 2017 07:47:52 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2017-08-14T07:47:52Z</dc:date>
    <item>
      <title>Protect the code</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Protect-the-code/m-p/698124#M8730</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would like to ask, I use the MPC5744, I would like to protect my code, for example, others get the source code can not be amended, if the amendment can not compile. What should I do?Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Aug 2017 05:36:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Protect-the-code/m-p/698124#M8730</guid>
      <dc:creator>boshimao</dc:creator>
      <dc:date>2017-08-14T05:36:11Z</dc:date>
    </item>
    <item>
      <title>Re: Protect the code</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Protect-the-code/m-p/698125#M8731</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I expect that you are talking about code encryption.&lt;/P&gt;&lt;P&gt;Unfortunately micro you have chosen does not support HW protection&amp;nbsp; like HSM (hardware security module) or CSE (cryptographic service engine).&lt;/P&gt;&lt;P&gt;On the other hand you can use Flash array integrity check to prevent any unintended code change. But one with source code can easily find and modify the code to skip this check.&lt;/P&gt;&lt;P&gt;It is common that customers use external cryptographic tools to encrypt generated binary output files. This is based on polynomial encrypting and it's quite hard to break these encryption tools.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Aug 2017 07:47:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Protect-the-code/m-p/698125#M8731</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-08-14T07:47:52Z</dc:date>
    </item>
    <item>
      <title>Re: Protect the code</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Protect-the-code/m-p/698126#M8732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;Can the compiler compile the code into a library file, and then someone else can only call.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Aug 2017 10:05:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Protect-the-code/m-p/698126#M8732</guid>
      <dc:creator>boshimao</dc:creator>
      <dc:date>2017-08-15T10:05:39Z</dc:date>
    </item>
  </channel>
</rss>