<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: Difference between MIOS and eMIOS</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Difference-between-MIOS-and-eMIOS/m-p/414227#M873</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;The MIOS was timer module used on MPC5xx parts, quite different from eMIOS/eMISO200. However was done on modular concept. There was up to six time base counter buses (modulus counter submodule), that provide counter buses&amp;nbsp; to up to 10 double action sub modules (DASM) which can be programmed for variour functions (Input capture, period &amp;amp; pulse width measurement, output compare, PWM). Moreover there was up to 12 Pulse Width Modulation Submodules with 0% and 100% duty cycle capability. &lt;/P&gt;&lt;P&gt;You can see MIOS description is some MPC5xx RM, for example &lt;A href="http://cache.freescale.com/files/microcontrollers/doc/ref_manual/MPC565RM.pdf"&gt;http://cache.freescale.com/files/microcontrollers/doc/ref_manual/MPC565RM.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;The eMIOS module, used on MPC55xx family, builds on the MIOS concept by using a unified channel module that provides a superset of the functionality of all the individual MIOS channels.&lt;/P&gt;&lt;P&gt;So there is up to 24 unified channels that all can be programmed to wide set of counting modes (Input capture, period &amp;amp; pulse width measurement, output compare, modulus conter normal/buffered, PWM normal/buffered), see e.g. &lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/MPC5567RM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/MPC5567RM.pdf&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The eMIOS200, used on newer devices - MPC56xx, is a general term for reduced version of eMIOS module. The only difference is that not all functions are available. It differs from device to device - usually there are several channels types/groups and these group offers only certain functions from the full eMIOS functions list.&lt;/P&gt;&lt;P&gt;You should always consult the device RM to know what functions are implemented on each channel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Jun 2015 06:47:24 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2015-06-19T06:47:24Z</dc:date>
    <item>
      <title>Difference between MIOS and eMIOS</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Difference-between-MIOS-and-eMIOS/m-p/414226#M872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; what is difference between MIOS, eMIOS&amp;nbsp; ,eMIOS200...give me brief explanation about eMIOS200..and how to work on it...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jun 2015 05:24:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Difference-between-MIOS-and-eMIOS/m-p/414226#M872</guid>
      <dc:creator>natarajmani</dc:creator>
      <dc:date>2015-06-19T05:24:23Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between MIOS and eMIOS</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Difference-between-MIOS-and-eMIOS/m-p/414227#M873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;The MIOS was timer module used on MPC5xx parts, quite different from eMIOS/eMISO200. However was done on modular concept. There was up to six time base counter buses (modulus counter submodule), that provide counter buses&amp;nbsp; to up to 10 double action sub modules (DASM) which can be programmed for variour functions (Input capture, period &amp;amp; pulse width measurement, output compare, PWM). Moreover there was up to 12 Pulse Width Modulation Submodules with 0% and 100% duty cycle capability. &lt;/P&gt;&lt;P&gt;You can see MIOS description is some MPC5xx RM, for example &lt;A href="http://cache.freescale.com/files/microcontrollers/doc/ref_manual/MPC565RM.pdf"&gt;http://cache.freescale.com/files/microcontrollers/doc/ref_manual/MPC565RM.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;The eMIOS module, used on MPC55xx family, builds on the MIOS concept by using a unified channel module that provides a superset of the functionality of all the individual MIOS channels.&lt;/P&gt;&lt;P&gt;So there is up to 24 unified channels that all can be programmed to wide set of counting modes (Input capture, period &amp;amp; pulse width measurement, output compare, modulus conter normal/buffered, PWM normal/buffered), see e.g. &lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/MPC5567RM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/MPC5567RM.pdf&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The eMIOS200, used on newer devices - MPC56xx, is a general term for reduced version of eMIOS module. The only difference is that not all functions are available. It differs from device to device - usually there are several channels types/groups and these group offers only certain functions from the full eMIOS functions list.&lt;/P&gt;&lt;P&gt;You should always consult the device RM to know what functions are implemented on each channel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jun 2015 06:47:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Difference-between-MIOS-and-eMIOS/m-p/414227#M873</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2015-06-19T06:47:24Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between MIOS and eMIOS</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Difference-between-MIOS-and-eMIOS/m-p/414228#M874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you friend,,how to use eMIOS for GPIO ....what is the use when we are using eMIOS for GPIO..need explanation and sample code for MPC5674f&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jun 2015 06:58:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Difference-between-MIOS-and-eMIOS/m-p/414228#M874</guid>
      <dc:creator>natarajmani</dc:creator>
      <dc:date>2015-06-19T06:58:16Z</dc:date>
    </item>
  </channel>
</rss>