<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCP5775 SDPLL can't lock when using external clock source in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MCP5775-SDPLL-can-t-lock-when-using-external-clock-source/m-p/693758#M8634</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using a 3.3v LVCMOS external clock source to drive MPC5775 now. The PLL0 can lock normally, but SDPLL can't lock. The code will always pending on&amp;nbsp;while(AFE.PLLSTS.B.LOCK == 0);&amp;nbsp;&lt;/P&gt;&lt;P&gt;The PLLSTS register show 0 on bit0, bit1, bit2 and bit15.&lt;/P&gt;&lt;P&gt;The code can lock correctly on the same board with a crystal. The only difference on code is &amp;nbsp;AFE.OSCCTRL.B.EN_EXT setting.&lt;/P&gt;&lt;P&gt;Would you please let me know that if I missed something to set?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Aug 2017 05:19:06 GMT</pubDate>
    <dc:creator>hqliu</dc:creator>
    <dc:date>2017-08-04T05:19:06Z</dc:date>
    <item>
      <title>MCP5775 SDPLL can't lock when using external clock source</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MCP5775-SDPLL-can-t-lock-when-using-external-clock-source/m-p/693758#M8634</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using a 3.3v LVCMOS external clock source to drive MPC5775 now. The PLL0 can lock normally, but SDPLL can't lock. The code will always pending on&amp;nbsp;while(AFE.PLLSTS.B.LOCK == 0);&amp;nbsp;&lt;/P&gt;&lt;P&gt;The PLLSTS register show 0 on bit0, bit1, bit2 and bit15.&lt;/P&gt;&lt;P&gt;The code can lock correctly on the same board with a crystal. The only difference on code is &amp;nbsp;AFE.OSCCTRL.B.EN_EXT setting.&lt;/P&gt;&lt;P&gt;Would you please let me know that if I missed something to set?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Aug 2017 05:19:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MCP5775-SDPLL-can-t-lock-when-using-external-clock-source/m-p/693758#M8634</guid>
      <dc:creator>hqliu</dc:creator>
      <dc:date>2017-08-04T05:19:06Z</dc:date>
    </item>
  </channel>
</rss>