<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5645s: Start-Up Issue</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5645s-Start-Up-Issue/m-p/692864#M8595</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;what does it means does not star?&lt;/P&gt;&lt;P&gt;It stays in reset?&lt;/P&gt;&lt;P&gt;reset periodical?&lt;/P&gt;&lt;P&gt;is stuck in program?&lt;/P&gt;&lt;P&gt;Do you service watchdog?&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Jul 2017 08:45:33 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2017-07-12T08:45:33Z</dc:date>
    <item>
      <title>MPC5645s: Start-Up Issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5645s-Start-Up-Issue/m-p/692863#M8594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am facing issue with startup of MPC5645s. I am able to run my application code on the micro using debugger but when I flash it and try to run (without debugger) then it does not start.&lt;/P&gt;&lt;P&gt;Any idea what could be the issue?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jul 2017 18:25:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5645s-Start-Up-Issue/m-p/692863#M8594</guid>
      <dc:creator>sagardhavali</dc:creator>
      <dc:date>2017-07-11T18:25:52Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5645s: Start-Up Issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5645s-Start-Up-Issue/m-p/692864#M8595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;what does it means does not star?&lt;/P&gt;&lt;P&gt;It stays in reset?&lt;/P&gt;&lt;P&gt;reset periodical?&lt;/P&gt;&lt;P&gt;is stuck in program?&lt;/P&gt;&lt;P&gt;Do you service watchdog?&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jul 2017 08:45:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5645s-Start-Up-Issue/m-p/692864#M8595</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-07-12T08:45:33Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5645s: Start-Up Issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5645s-Start-Up-Issue/m-p/692865#M8596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what does it means does not star?&lt;/P&gt;&lt;P&gt;- It does not start to run but it does run when executed with emulator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It stays in reset?&lt;/P&gt;&lt;P&gt;- It looks like so, We are investigating that. But question is, if it is in Reset, it should not have run from emulator too but it runs perfectly as expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reset periodical?&lt;/P&gt;&lt;P&gt;- No, it is not periodical. It is not that it start and stops. It does not start at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is stuck in program?&lt;/P&gt;&lt;P&gt;- No. If it was stuck in program, at list power LED should have turned at least once. It does not start at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you service watchdog?&lt;/P&gt;&lt;P&gt;- It is disabled at the moment to bring up the functionality.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jul 2017 15:00:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5645s-Start-Up-Issue/m-p/692865#M8596</guid>
      <dc:creator>sagardhavali</dc:creator>
      <dc:date>2017-07-12T15:00:12Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5645s: Start-Up Issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5645s-Start-Up-Issue/m-p/692866#M8597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So let me summarize:&lt;/P&gt;&lt;P&gt;1. It is not running as standalone. Correct?&lt;/P&gt;&lt;P&gt;2. You don't know if device stay in reset or no. -&amp;gt; check Reset_B pin.&lt;/P&gt;&lt;P&gt;3. Did you check it with scope to verify if it is not periodical?&lt;/P&gt;&lt;P&gt;4. Watchdog is disabled by debugger, but if you do not disable/service it in your startup the device will end up in reset escalation.&lt;/P&gt;&lt;P&gt;Anyway, if you are able to connect with debugger after failure in standalone mode you can check RGM FES/DES registers to find reset root cause.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can check your code if you can share your binary with me.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: You mismatch the meaning of debug probe and emulator.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jul 2017 07:41:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5645s-Start-Up-Issue/m-p/692866#M8597</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-07-13T07:41:09Z</dc:date>
    </item>
  </channel>
</rss>