<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32R274RRUEVB startup in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/S32R274RRUEVB-startup/m-p/691022#M8549</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply and comments.&lt;/P&gt;&lt;P&gt;For my test bench, I have 5V and 3.3V regulated DC supply only, I noticed&lt;/P&gt;&lt;P&gt;there is a on board SMPS FET on the S32R274RRUEVB schematic that supplies&lt;/P&gt;&lt;P&gt;1.25V core supply for the micro, my question is if I can use this on board&lt;/P&gt;&lt;P&gt;SMPS and negate the 1.25V_DC_R from the J1-PWR_IN connector. if yes, how&lt;/P&gt;&lt;P&gt;should I configure the jumpers accordingly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Qi Yuan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Aug 2017 08:22:55 GMT</pubDate>
    <dc:creator>qiyuan</dc:creator>
    <dc:date>2017-08-10T08:22:55Z</dc:date>
    <item>
      <title>S32R274RRUEVB startup</title>
      <link>https://community.nxp.com/t5/MPC5xxx/S32R274RRUEVB-startup/m-p/691020#M8547</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I just got my S32R274RRUEVB board from NXP.&lt;/P&gt;&lt;P&gt;There are 3 power supply terminals on this board, do I have to connect them all to power up this daughter board alone as I don't have the motherboard? they are:&lt;/P&gt;&lt;P&gt;5V_DC_R&lt;/P&gt;&lt;P&gt;3.3V_DC_R&lt;/P&gt;&lt;P&gt;1.25V_DC_R&lt;/P&gt;&lt;P&gt;From the schematic, it looks like 1.25V can be internally supplied thru 5V_DC_R, what about the 3.3V_SR_LDO? can I just supply a single 5V supply externally to power up the board to do some simple test?&lt;/P&gt;&lt;P&gt;Is there any user manual to start with?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Aug 2017 06:13:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/S32R274RRUEVB-startup/m-p/691020#M8547</guid>
      <dc:creator>qiyuan</dc:creator>
      <dc:date>2017-08-02T06:13:31Z</dc:date>
    </item>
    <item>
      <title>Re: S32R274RRUEVB startup</title>
      <link>https://community.nxp.com/t5/MPC5xxx/S32R274RRUEVB-startup/m-p/691021#M8548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is possible to use the daughter cards without the motherboard to run code on the microcontroller.&lt;/P&gt;&lt;P&gt;Power to the daughter cards must be supplied through the terminal power connector ‘J1 – PWR_IN’. It&lt;/P&gt;&lt;P&gt;is required to connect all three voltages (1.25V, 3.3V and 5V) and ground.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jumpers positions must be moved to allow the J1 to supply the EVB.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;J3 must move to position 1-2&amp;nbsp;&amp;nbsp; (5V_DC_R)&lt;/P&gt;&lt;P&gt;J2 must move to position 1-2&amp;nbsp;&amp;nbsp; (1.25V_DC_R)&lt;/P&gt;&lt;P&gt;J7 must move to position 1-2&amp;nbsp;&amp;nbsp; (5V_DC_R)&lt;/P&gt;&lt;P&gt;J5 must move to position 1-2&amp;nbsp;&amp;nbsp; (3.3V_DC_R)&lt;/P&gt;&lt;P&gt;J4 must move to position 1-2&amp;nbsp;&amp;nbsp; (5V_DC_R)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Aug 2017 11:32:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/S32R274RRUEVB-startup/m-p/691021#M8548</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-08-09T11:32:34Z</dc:date>
    </item>
    <item>
      <title>Re: S32R274RRUEVB startup</title>
      <link>https://community.nxp.com/t5/MPC5xxx/S32R274RRUEVB-startup/m-p/691022#M8549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply and comments.&lt;/P&gt;&lt;P&gt;For my test bench, I have 5V and 3.3V regulated DC supply only, I noticed&lt;/P&gt;&lt;P&gt;there is a on board SMPS FET on the S32R274RRUEVB schematic that supplies&lt;/P&gt;&lt;P&gt;1.25V core supply for the micro, my question is if I can use this on board&lt;/P&gt;&lt;P&gt;SMPS and negate the 1.25V_DC_R from the J1-PWR_IN connector. if yes, how&lt;/P&gt;&lt;P&gt;should I configure the jumpers accordingly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Qi Yuan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Aug 2017 08:22:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/S32R274RRUEVB-startup/m-p/691022#M8549</guid>
      <dc:creator>qiyuan</dc:creator>
      <dc:date>2017-08-10T08:22:55Z</dc:date>
    </item>
  </channel>
</rss>