<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックMPC5602P to MPC5605B</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5602P-to-MPC5605B/m-p/412604#M853</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I currently have a running software bootloader on MPC5602P and I want to port it to MPC5605B. I have tried to simply download the binary file in the chip and it seems to work fine so I guess it's not to complicated.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried to copy the project and change the headers. I also have try to start a new project and copy the code but it doesn't work neither. I think my issue is related to the use of the shadow memory.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the classic codewarrior, there is a way to change the derivative for a project. Is there something similar with eclipse? What is the best way to migrate my code from these two chip from the same family?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Jun 2015 13:54:58 GMT</pubDate>
    <dc:creator>ZdenoQC</dc:creator>
    <dc:date>2015-06-18T13:54:58Z</dc:date>
    <item>
      <title>MPC5602P to MPC5605B</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5602P-to-MPC5605B/m-p/412604#M853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I currently have a running software bootloader on MPC5602P and I want to port it to MPC5605B. I have tried to simply download the binary file in the chip and it seems to work fine so I guess it's not to complicated.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried to copy the project and change the headers. I also have try to start a new project and copy the code but it doesn't work neither. I think my issue is related to the use of the shadow memory.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the classic codewarrior, there is a way to change the derivative for a project. Is there something similar with eclipse? What is the best way to migrate my code from these two chip from the same family?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2015 13:54:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5602P-to-MPC5605B/m-p/412604#M853</guid>
      <dc:creator>ZdenoQC</dc:creator>
      <dc:date>2015-06-18T13:54:58Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5602P to MPC5605B</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5602P-to-MPC5605B/m-p/412605#M854</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi William,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The best way is just to create a new project for MPC5605B.&lt;/P&gt;&lt;P&gt;Set all the includes, optimalizations, project settings, etc... for MOC5605B and compile this project.&lt;/P&gt;&lt;P&gt;Then start porting:&lt;/P&gt;&lt;P&gt;Start adding the functions, definitions, variables, etc... from original project and make sure you can compile them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you do everything in correct way the project must run on MPC5605B with no issues.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jun 2015 11:30:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5602P-to-MPC5605B/m-p/412605#M854</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2015-06-23T11:30:04Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5602P to MPC5605B</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5602P-to-MPC5605B/m-p/412606#M855</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the answer Peter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My issue was with the target task. Since I use the shadow flash, I need a custom configuration to program the bootloader. Since I was not the one who develop this part it take me sometime to figure it out. I also have to force the bootmap to start in shadow flash instead of the ram of my application by changing the generated binary file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyway it working now&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2015 20:26:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5602P-to-MPC5605B/m-p/412606#M855</guid>
      <dc:creator>ZdenoQC</dc:creator>
      <dc:date>2015-07-08T20:26:04Z</dc:date>
    </item>
  </channel>
</rss>