<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5645S with external oscillator  in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5645S-with-external-oscillator/m-p/690624#M8528</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I apologize , i wrote an error&amp;nbsp;&amp;nbsp;in my post , i was talking about EXTAL as an entry&amp;nbsp;for the oscillator ,and XTAL is not connected.&lt;/P&gt;&lt;P&gt;The oscillator is really connected on the EXTAL entry &amp;nbsp;an XTAL is left non connected.&lt;/P&gt;&lt;P&gt;But it doesn'twork...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pierre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Aug 2017 11:41:34 GMT</pubDate>
    <dc:creator>PCC</dc:creator>
    <dc:date>2017-08-02T11:41:34Z</dc:date>
    <item>
      <title>MPC5645S with external oscillator</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5645S-with-external-oscillator/m-p/690622#M8526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The cpu runs correctly with 16MHz internal RC , we want to use the internal &amp;nbsp;PLL with connecting an&amp;nbsp;&amp;nbsp;External oscillator 8MHZ&lt;/P&gt;&lt;P&gt;=&amp;gt; the cpu doesnt start correctly because it&amp;nbsp;detects&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;S_FXOSC =0&lt;/STRONG&gt; (0 fast external crystal oscillator (4-16 MHz) is not stable)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the oscillator is &amp;nbsp;MASTERCRISTAL MCS01Y-B-8MHZ &amp;nbsp;level is 1,2V , square wave is clean , stable and accurate 8MHZ&lt;/P&gt;&lt;P&gt;The trace of XTAL is short (3.5mm) , the EXTAL is left unconnected (we try too with EXTAL grounded )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With 2 différents boards , the problem is the same&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can any body help us ?&lt;/P&gt;&lt;P&gt;Thanks for all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pierre CAZENAVE&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Aug 2017 09:54:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5645S-with-external-oscillator/m-p/690622#M8526</guid>
      <dc:creator>PCC</dc:creator>
      <dc:date>2017-08-02T09:54:12Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5645S with external oscillator</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5645S-with-external-oscillator/m-p/690623#M8527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pierre,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;clock should be connected to the EXTAL pin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/8461i123F4FB72A6DEF48/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Aug 2017 10:12:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5645S-with-external-oscillator/m-p/690623#M8527</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-08-02T10:12:17Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5645S with external oscillator</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5645S-with-external-oscillator/m-p/690624#M8528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I apologize , i wrote an error&amp;nbsp;&amp;nbsp;in my post , i was talking about EXTAL as an entry&amp;nbsp;for the oscillator ,and XTAL is not connected.&lt;/P&gt;&lt;P&gt;The oscillator is really connected on the EXTAL entry &amp;nbsp;an XTAL is left non connected.&lt;/P&gt;&lt;P&gt;But it doesn'twork...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pierre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Aug 2017 11:41:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5645S-with-external-oscillator/m-p/690624#M8528</guid>
      <dc:creator>PCC</dc:creator>
      <dc:date>2017-08-02T11:41:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5645S with external oscillator</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5645S-with-external-oscillator/m-p/690625#M8529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the same problem, do you find the solution to this problem Pierre ?&lt;/P&gt;&lt;P&gt;The crystal configuration works fine, but it doesn't work with only an oscillator on the EXTAL pin and nothing on the XTAL pin.&lt;/P&gt;&lt;P&gt;I have maid the same circuit on a MPC5646C and it works !&lt;/P&gt;&lt;P&gt;Is the MPC5645S more sensitive ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Feb 2018 11:04:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5645S-with-external-oscillator/m-p/690625#M8529</guid>
      <dc:creator>robinauriol</dc:creator>
      <dc:date>2018-02-23T11:04:01Z</dc:date>
    </item>
  </channel>
</rss>