<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: Can't program UTest in MPC5748G</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Can-t-program-UTest-in-MPC5748G/m-p/685125#M8355</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;UPDATE: we&amp;nbsp;eventually found a workaround: instead of advancing the life cycle setting to In Field we advanced it to OEM Production (which is a single step forward; that might have been the issue).&lt;/P&gt;&lt;P&gt;Like Peter mentions, we also needed to add a DCF with censorship mode and set the password groups and password group locks (also as DCFs) appropriately.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Jul 2017 14:00:46 GMT</pubDate>
    <dc:creator>alexeikovelman</dc:creator>
    <dc:date>2017-07-12T14:00:46Z</dc:date>
    <item>
      <title>Can't program UTest in MPC5748G</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Can-t-program-UTest-in-MPC5748G/m-p/685122#M8352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to program the UTest area of the MPC5748G MCU.&lt;BR /&gt;In particular I'm trying to enable password protection for the JTAG interface, so I'm trying to set the JTAG password field and the life cycle fields in the UTest flash area.&lt;/P&gt;&lt;P&gt;The trouble seems to be that only the JTAG password is written but the life cycle areas aren't - and since UTest is OTP I can only try once per board.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My Lauterbach script and the UTest memory dump are&amp;nbsp;attached.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Two questions:&lt;BR /&gt; - any idea&amp;nbsp;why the script doesn't work as expected?&lt;BR /&gt; - is there another way (that I missed) to enable password protection for the JTAG interface?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338345"&gt;MPC5744P_DCF_Censorship_ours.cmm.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338345"&gt;MPC5744P_DCF_Censorship_ours_fixed.cmm.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jul 2017 13:53:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Can-t-program-UTest-in-MPC5748G/m-p/685122#M8352</guid>
      <dc:creator>alexeikovelman</dc:creator>
      <dc:date>2017-07-05T13:53:40Z</dc:date>
    </item>
    <item>
      <title>Re: Can't program UTest in MPC5748G</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Can-t-program-UTest-in-MPC5748G/m-p/685123#M8353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Its hard to say what is wrong as you didn't attach dump of your UTEST memory.&lt;/P&gt;&lt;P&gt;Anyway, here is reference script for censorship programing and also separate one for only life cycle programming.&lt;/P&gt;&lt;P&gt;As UTEST is OTP, make sure first that you really understand censorship of this device.&lt;/P&gt;&lt;P&gt;Or use the board with socket where you can easily exchange micro.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jul 2017 08:05:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Can-t-program-UTest-in-MPC5748G/m-p/685123#M8353</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-07-11T08:05:08Z</dc:date>
    </item>
    <item>
      <title>Re: Can't program UTest in MPC5748G</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Can-t-program-UTest-in-MPC5748G/m-p/685124#M8354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter,&lt;/P&gt;&lt;P&gt;I've edited the original post to include the UTest memory dump; does this lead you to a different conclusion?&lt;/P&gt;&lt;P&gt;Meanwhile I'll take a look at your scripts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, we found a bug in the addresses we used in the script, but fixing them didn't change the outcome; the script in the original post includes the fix.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jul 2017 10:43:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Can-t-program-UTest-in-MPC5748G/m-p/685124#M8354</guid>
      <dc:creator>alexeikovelman</dc:creator>
      <dc:date>2017-07-11T10:43:53Z</dc:date>
    </item>
    <item>
      <title>Re: Can't program UTest in MPC5748G</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Can-t-program-UTest-in-MPC5748G/m-p/685125#M8355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;UPDATE: we&amp;nbsp;eventually found a workaround: instead of advancing the life cycle setting to In Field we advanced it to OEM Production (which is a single step forward; that might have been the issue).&lt;/P&gt;&lt;P&gt;Like Peter mentions, we also needed to add a DCF with censorship mode and set the password groups and password group locks (also as DCFs) appropriately.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jul 2017 14:00:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Can-t-program-UTest-in-MPC5748G/m-p/685125#M8355</guid>
      <dc:creator>alexeikovelman</dc:creator>
      <dc:date>2017-07-12T14:00:46Z</dc:date>
    </item>
    <item>
      <title>Re: Can't program UTest in MPC5748G</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Can-t-program-UTest-in-MPC5748G/m-p/685126#M8356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One more thing:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27017i479596AC9ECE416F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;in customer deliver censorship is don't care. But censorship register is programmed in factory to value other the 0x55AA.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27059i0F1ACF44EBADF890/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So if you migrate to OEM production you have to program censorship register otherwise you will get your device bricked.&lt;/P&gt;&lt;P&gt;Or you must program valid JTAG password.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jul 2017 08:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Can-t-program-UTest-in-MPC5748G/m-p/685126#M8356</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-07-18T08:27:03Z</dc:date>
    </item>
  </channel>
</rss>