<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5643L IRC Accuracy</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5643L-IRC-Accuracy/m-p/682956#M8258</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think I know the reason. Even though it is not described in MPC5643L, I have found description in RM of other device where I am almost sure it works the same way:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3i4D35FEA2451E9675/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Try to comment mentioned RAppID trimming&lt;/P&gt;&lt;P&gt;&lt;EM&gt;CGM.RC_CTL.R = 0x00000000;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; /* IRC Oscillator Trimming: 0 */&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe it helps. If you confirm it to me I will report it to competent person.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Jul 2017 11:38:27 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2017-07-27T11:38:27Z</dc:date>
    <item>
      <title>MPC5643L IRC Accuracy</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5643L-IRC-Accuracy/m-p/682953#M8255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;During some recent testing of the CMU I discovered that the high/low limits that I had set for the system clock were not working as expected. Some further experiments have concluded that the problem was that the IRC (measured on several devices using several methods - CLKOUT pin, CMU frequency measurement and reverse calculating IRC from CMU using the tightest high/low limits that didn't cause a reset) was somewhere between 13-14Mhz instead of the expected 16MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm aware that the internal oscillators are not necessarily known for their accuracy, but various datasheets refer to the worst case accuracy range for this device to be +/-6%, whereas I'm seeing between 12-18% on a number of relatively new devices at room temperature.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an explanation for this behaviour?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Jul 2017 13:11:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5643L-IRC-Accuracy/m-p/682953#M8255</guid>
      <dc:creator>martinp</dc:creator>
      <dc:date>2017-07-25T13:11:00Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5643L IRC Accuracy</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5643L-IRC-Accuracy/m-p/682954#M8256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, does you code touch RC_CTL register? What is your RC_CTL content?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/28797iA03CA1EC28E51CB3/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2017 10:06:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5643L-IRC-Accuracy/m-p/682954#M8256</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2017-07-27T10:06:13Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5643L IRC Accuracy</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5643L-IRC-Accuracy/m-p/682955#M8257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, RC_CTL is&amp;nbsp;set by RAppID setup code to 0 and left untouched after that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt; CGM.RC_CTL.R = 0x00000000;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; /* IRC Oscillator Trimming: 0 */&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2017 10:13:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5643L-IRC-Accuracy/m-p/682955#M8257</guid>
      <dc:creator>martinp</dc:creator>
      <dc:date>2017-07-27T10:13:35Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5643L IRC Accuracy</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5643L-IRC-Accuracy/m-p/682956#M8258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think I know the reason. Even though it is not described in MPC5643L, I have found description in RM of other device where I am almost sure it works the same way:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3i4D35FEA2451E9675/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Try to comment mentioned RAppID trimming&lt;/P&gt;&lt;P&gt;&lt;EM&gt;CGM.RC_CTL.R = 0x00000000;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; /* IRC Oscillator Trimming: 0 */&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe it helps. If you confirm it to me I will report it to competent person.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2017 11:38:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5643L-IRC-Accuracy/m-p/682956#M8258</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2017-07-27T11:38:27Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5643L IRC Accuracy</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5643L-IRC-Accuracy/m-p/682957#M8259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've just done a quick test, commenting that line out as suggested, and it does seem to have fixed the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll keep investigating to make sure and will reply if there are any other issues, but it's looking good for now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2017 12:44:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5643L-IRC-Accuracy/m-p/682957#M8259</guid>
      <dc:creator>martinp</dc:creator>
      <dc:date>2017-07-27T12:44:45Z</dc:date>
    </item>
  </channel>
</rss>