<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5777M IO in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-IO/m-p/681348#M8199</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One more thing I want to add.&lt;/P&gt;&lt;P&gt;Maybe it is not 100% clear from reference manual.&lt;/P&gt;&lt;P&gt;The device could work with IO at 3.3V, however during reset phase 0 to 3 the&amp;nbsp; LVD400 (4V LVD) is active by default.&lt;/P&gt;&lt;P&gt;So if you want to run IO at 3.3V you have to start with 5V on VDD_HV_IO_MAIN and when device reach phase 3 o reset you can configure via DCF records LVD400 (turn it off). After this point you can switch to 3.3V IO supply.&lt;/P&gt;&lt;P&gt;Otherwise the LVD400 will keep device in reset as 3.3V will always be treated as undervoltage event by LVD400.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Jun 2017 04:38:27 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2017-06-12T04:38:27Z</dc:date>
    <item>
      <title>MPC5777M IO</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-IO/m-p/681346#M8197</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to supply IO with 3.3V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Jun 2017 06:31:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777M-IO/m-p/681346#M8197</guid>
      <dc:creator>even</dc:creator>
      <dc:date>2017-06-09T06:31:39Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777M IO</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-IO/m-p/681347#M8198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yes, it is possible to supply VDD_HV_IO with 3.3V.&lt;/P&gt;&lt;P&gt;However make sure you correctly understand the voltage detectors. Especially LVD400_IM which has to be disabled in order to prevent unintended resets from LVD at 4V.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Jun 2017 20:02:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777M-IO/m-p/681347#M8198</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-06-11T20:02:47Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777M IO</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-IO/m-p/681348#M8199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One more thing I want to add.&lt;/P&gt;&lt;P&gt;Maybe it is not 100% clear from reference manual.&lt;/P&gt;&lt;P&gt;The device could work with IO at 3.3V, however during reset phase 0 to 3 the&amp;nbsp; LVD400 (4V LVD) is active by default.&lt;/P&gt;&lt;P&gt;So if you want to run IO at 3.3V you have to start with 5V on VDD_HV_IO_MAIN and when device reach phase 3 o reset you can configure via DCF records LVD400 (turn it off). After this point you can switch to 3.3V IO supply.&lt;/P&gt;&lt;P&gt;Otherwise the LVD400 will keep device in reset as 3.3V will always be treated as undervoltage event by LVD400.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jun 2017 04:38:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777M-IO/m-p/681348#M8199</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-06-12T04:38:27Z</dc:date>
    </item>
  </channel>
</rss>