<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5744 FCCU Initialization Issue in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5744-FCCU-Initialization-Issue/m-p/681224#M8191</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;NCF[12] is caused by RCCU fault which represent lock-step error on D-MEM controller which is replicated in safety lake.&lt;/P&gt;&lt;P&gt;Usually I do FCCU init in main as first called function.&lt;/P&gt;&lt;P&gt;But in safety systems it should be done when device is ready to execute safety tasks.&lt;/P&gt;&lt;P&gt;After Power on Reset, when second core is activated during reset phase (via DCF record) then RCCU faults can occur.&lt;/P&gt;&lt;P&gt;Clear the faults and if the RCCU fault is also present after other then POReset then you must analyze it.&lt;/P&gt;&lt;P&gt;If the fault is present only After POR then it is caused by delayed activation of core and makes no sense to analyze this fault.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 May 2017 12:33:45 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2017-05-16T12:33:45Z</dc:date>
    <item>
      <title>MPC5744 FCCU Initialization Issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744-FCCU-Initialization-Issue/m-p/681223#M8190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What conditions can lead to&amp;nbsp;the occurrence of FCCU NCF[12] (&amp;nbsp;Core redundancy mismatch: D-MEM array interface out of lockstep ) ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to AN5259: "The root cause can be a permanent fault or a transient fault (either in the safety lake or in the original lake) that propagated to any outputs of the lake."&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Currently, when we change time in which FCCU is initialized. FCCU goes into ALARM state because of NCF[12] and goes back again into NORMAL state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could it be a fault in Lockstep Core and not in Core 0 or might it be the cores aren't completely synchronized during initialization. In other words, what could be the reasons behind this FCCU fault ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, from your experience, in a standard AUTOSAR environment initialization sequence:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="EcuM_Initialization.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19193i144BC2387E1554D5/image-size/large?v=v2&amp;amp;px=999" role="button" title="EcuM_Initialization.PNG" alt="EcuM_Initialization.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The problem basically happens when we move FCCU init to any Init Block other than Init Block III.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is your recommendation when the FCCU initialization should take place ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ahmed&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 May 2017 09:24:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744-FCCU-Initialization-Issue/m-p/681223#M8190</guid>
      <dc:creator>ahmedsoubky</dc:creator>
      <dc:date>2017-05-16T09:24:04Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744 FCCU Initialization Issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744-FCCU-Initialization-Issue/m-p/681224#M8191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;NCF[12] is caused by RCCU fault which represent lock-step error on D-MEM controller which is replicated in safety lake.&lt;/P&gt;&lt;P&gt;Usually I do FCCU init in main as first called function.&lt;/P&gt;&lt;P&gt;But in safety systems it should be done when device is ready to execute safety tasks.&lt;/P&gt;&lt;P&gt;After Power on Reset, when second core is activated during reset phase (via DCF record) then RCCU faults can occur.&lt;/P&gt;&lt;P&gt;Clear the faults and if the RCCU fault is also present after other then POReset then you must analyze it.&lt;/P&gt;&lt;P&gt;If the fault is present only After POR then it is caused by delayed activation of core and makes no sense to analyze this fault.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 May 2017 12:33:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744-FCCU-Initialization-Issue/m-p/681224#M8191</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-05-16T12:33:45Z</dc:date>
    </item>
  </channel>
</rss>