<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5775K FlexCAN Loopback module</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-FlexCAN-Loopback-module/m-p/674643#M7902</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need not change the state of pins. The loopback mode is used for internal test, for example testing of receive/masking operation. FlexCAN behaves as it normally does when transmitting and treats its own transmitted message as a message received from a remote node. The ACK field is ignored so the message can be received normally.&lt;/P&gt;&lt;P&gt;In the loopback mode no message is visible on TX output, it goes to the recessive state (logic “1”).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Jun 2017 06:17:22 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2017-06-06T06:17:22Z</dc:date>
    <item>
      <title>MPC5775K FlexCAN Loopback module</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-FlexCAN-Loopback-module/m-p/674642#M7901</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I'm using MPC5775K to test FlexCAN module now,but I have a lot of questions in the loopback mode,the datasheet said that&amp;nbsp;The Rx CAN input pin is ignored and the Tx CAN output goes to the recessive state (logic '1'),does it means that after I transmit &amp;nbsp;a frame of data ,I should change the state of&amp;nbsp;&lt;SPAN&gt;Tx from output to input? Thank you!!!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jun 2017 09:59:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-FlexCAN-Loopback-module/m-p/674642#M7901</guid>
      <dc:creator>lihongrun</dc:creator>
      <dc:date>2017-06-05T09:59:51Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775K FlexCAN Loopback module</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775K-FlexCAN-Loopback-module/m-p/674643#M7902</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need not change the state of pins. The loopback mode is used for internal test, for example testing of receive/masking operation. FlexCAN behaves as it normally does when transmitting and treats its own transmitted message as a message received from a remote node. The ACK field is ignored so the message can be received normally.&lt;/P&gt;&lt;P&gt;In the loopback mode no message is visible on TX output, it goes to the recessive state (logic “1”).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jun 2017 06:17:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775K-FlexCAN-Loopback-module/m-p/674643#M7902</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-06-06T06:17:22Z</dc:date>
    </item>
  </channel>
</rss>