<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックidentifier 'int16_t' redeclared</title>
    <link>https://community.nxp.com/t5/MPC5xxx/identifier-int16-t-redeclared/m-p/673876#M7880</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using eclipse based code warrior IDE for MPC5604S controller. When I am building I get lot of warning mentioning that "identifier 'int16_t' redeclared ". I understood that my own project is also having the header files of '&lt;SPAN&gt;int16_t'&lt;/SPAN&gt;&amp;nbsp;which is creating this warning. But I need the header files which I provide and don't want to take from the installation folder. So how can I neglect the header file in the installation folder. Is there any settings in IDE to do this. Kindly provide some input ASAP.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 May 2017 10:04:37 GMT</pubDate>
    <dc:creator>akhilprasad</dc:creator>
    <dc:date>2017-05-10T10:04:37Z</dc:date>
    <item>
      <title>identifier 'int16_t' redeclared</title>
      <link>https://community.nxp.com/t5/MPC5xxx/identifier-int16-t-redeclared/m-p/673876#M7880</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using eclipse based code warrior IDE for MPC5604S controller. When I am building I get lot of warning mentioning that "identifier 'int16_t' redeclared ". I understood that my own project is also having the header files of '&lt;SPAN&gt;int16_t'&lt;/SPAN&gt;&amp;nbsp;which is creating this warning. But I need the header files which I provide and don't want to take from the installation folder. So how can I neglect the header file in the installation folder. Is there any settings in IDE to do this. Kindly provide some input ASAP.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 May 2017 10:04:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/identifier-int16-t-redeclared/m-p/673876#M7880</guid>
      <dc:creator>akhilprasad</dc:creator>
      <dc:date>2017-05-10T10:04:37Z</dc:date>
    </item>
    <item>
      <title>Re: identifier 'int16_t' redeclared</title>
      <link>https://community.nxp.com/t5/MPC5xxx/identifier-int16-t-redeclared/m-p/673877#M7881</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;these data types are declared in typedefs.h file placed in Project_headers folder. So, if you exclude this file from your project and use your own file, where you define your data types, the warning should disappear.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 May 2017 12:13:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/identifier-int16-t-redeclared/m-p/673877#M7881</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2017-05-16T12:13:44Z</dc:date>
    </item>
  </channel>
</rss>