<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5554 SW Image Footprints</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5554-SW-Image-Footprints/m-p/672433#M7841</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Are you referring to compiler output files?&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Jun 2017 13:01:23 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2017-06-06T13:01:23Z</dc:date>
    <item>
      <title>MPC5554 SW Image Footprints</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5554-SW-Image-Footprints/m-p/672432#M7840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What are the types and formats of Software footprint images supported by &amp;nbsp;MPC5554 Processor ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which is the best one among all these in terms of size?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jun 2017 05:12:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5554-SW-Image-Footprints/m-p/672432#M7840</guid>
      <dc:creator>shankarlingam</dc:creator>
      <dc:date>2017-06-02T05:12:33Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5554 SW Image Footprints</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5554-SW-Image-Footprints/m-p/672433#M7841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Are you referring to compiler output files?&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jun 2017 13:01:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5554-SW-Image-Footprints/m-p/672433#M7841</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-06-06T13:01:23Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5554 SW Image Footprints</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5554-SW-Image-Footprints/m-p/672434#M7842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is sort of that clarification. Basically we have S series of format in compilation and then produce ELF file format out of the S format specification.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is basically on which of the following types of the format that supports MPC 5554 processor platform and which one occupies the minimum memory utilization.?&lt;/P&gt;&lt;P&gt;Which is the best S format in terms of Size reduction?&lt;/P&gt;&lt;P&gt;Which is the best format of foot print image file having less size ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 07:53:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5554-SW-Image-Footprints/m-p/672434#M7842</guid>
      <dc:creator>shankarlingam</dc:creator>
      <dc:date>2017-06-07T07:53:26Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5554 SW Image Footprints</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5554-SW-Image-Footprints/m-p/672435#M7843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The size of output file depends on compiler optimization options.&lt;/P&gt;&lt;P&gt;This has nothing to do with output file format.&lt;/P&gt;&lt;P&gt;If you set compiler options to max size optimizations then you will get file which could execute code slower but its size is smaller.&lt;/P&gt;&lt;P&gt;I recommend you to always consult the compiler optimization with your compiler vendor.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 09:07:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5554-SW-Image-Footprints/m-p/672435#M7843</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-06-07T09:07:28Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5554 SW Image Footprints</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5554-SW-Image-Footprints/m-p/672436#M7844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I know the benefits of using SREC format.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;S19-style 16-bit address record&lt;/P&gt;&lt;P&gt;S28-style 24-bit address records&lt;/P&gt;&lt;P&gt;S37-style 32-bit address records&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I plan to use S37 style in stead of S19 style, &amp;nbsp;applying the&amp;nbsp;same set of command&amp;nbsp;for compilation, will there be any benefits in Size of the compiler output file?.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any alternative format other than&amp;nbsp;.ELF image file supported by MPC5554 processor?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jun 2017 05:54:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5554-SW-Image-Footprints/m-p/672436#M7844</guid>
      <dc:creator>shankarlingam</dc:creator>
      <dc:date>2017-06-08T05:54:40Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5554 SW Image Footprints</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5554-SW-Image-Footprints/m-p/672437#M7845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you pls clarify the my doubts given in above&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which SREC format is the best? Or it is simply thee representation of the file.&lt;/P&gt;&lt;P style="padding: 0px; min-height: 8pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;S19-style 16-bit address record&lt;/P&gt;&lt;P&gt;S28-style 24-bit address records&lt;/P&gt;&lt;P&gt;S37-style 32-bit address records&lt;/P&gt;&lt;P style="padding: 0px; min-height: 8pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I plan to use S37 style in stead of S19 style, &amp;nbsp;applying the&amp;nbsp;same set of command&amp;nbsp;for compilation, will there be any benefits in Size of the compiler output file?.&lt;/P&gt;&lt;P style="padding: 0px; min-height: 8pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any alternative format other than&amp;nbsp;.ELF image file supported by MPC5554 processor?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 16:45:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5554-SW-Image-Footprints/m-p/672437#M7845</guid>
      <dc:creator>shankarlingam</dc:creator>
      <dc:date>2017-06-13T16:45:06Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5554 SW Image Footprints</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5554-SW-Image-Footprints/m-p/672438#M7846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Are you referring to size of the file or size of the data in micro?&lt;/P&gt;&lt;P&gt;Customers usually use s3record file.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jun 2017 13:11:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5554-SW-Image-Footprints/m-p/672438#M7846</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-06-14T13:11:57Z</dc:date>
    </item>
  </channel>
</rss>