<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: BAF (Boot Assit Flash) erased. Is that possible ?</title>
    <link>https://community.nxp.com/t5/MPC5xxx/BAF-Boot-Assit-Flash-erased-Is-that-possible/m-p/403878#M754</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes it is possible to erase BAF.&lt;/P&gt;&lt;P&gt;To reload the BAF, dump it from sample with not erased BAF and flash it to erased sample.&lt;/P&gt;&lt;P&gt;Everything will work as expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Oct 2015 07:40:24 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2015-10-20T07:40:24Z</dc:date>
    <item>
      <title>BAF (Boot Assit Flash) erased. Is that possible ?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/BAF-Boot-Assit-Flash-erased-Is-that-possible/m-p/403877#M753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Freescale community,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working on MPC5746C, to develop a FLASH driver.&lt;/P&gt;&lt;P&gt;And it works too well, because it seems I erased the BAF block location (at 0x00400000).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now, when I flash and debug, the code entry&amp;nbsp; 0x00404100 is empty...&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;MPC5747G_RM_Rev4 says about the BAF:&lt;/P&gt;&lt;P&gt;"It is one time programmable (OTP) and is programmed during factory test."&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I am surprised that I was able to delete this area.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So is this case possible ?&lt;/P&gt;&lt;P&gt;Can I reload the BAF ? how to do so ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note I can manually set the PC to __entry, and then the code runs as it should.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN style="color: #000000; font-size: 14pt; font-family: TimesLTStd-Roman;"&gt; &lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Oct 2015 09:25:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/BAF-Boot-Assit-Flash-erased-Is-that-possible/m-p/403877#M753</guid>
      <dc:creator>stephanedemots</dc:creator>
      <dc:date>2015-10-16T09:25:20Z</dc:date>
    </item>
    <item>
      <title>Re: BAF (Boot Assit Flash) erased. Is that possible ?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/BAF-Boot-Assit-Flash-erased-Is-that-possible/m-p/403878#M754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes it is possible to erase BAF.&lt;/P&gt;&lt;P&gt;To reload the BAF, dump it from sample with not erased BAF and flash it to erased sample.&lt;/P&gt;&lt;P&gt;Everything will work as expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Oct 2015 07:40:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/BAF-Boot-Assit-Flash-erased-Is-that-possible/m-p/403878#M754</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2015-10-20T07:40:24Z</dc:date>
    </item>
  </channel>
</rss>