<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem with Initialize RAM in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Problem-with-Initialize-RAM/m-p/666862#M7527</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Asynchronous reset will possibly corrupt SRAM if it asserts during a read or write operation to SRAM. &lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;The completion of that access depends on the cycle at which the reset occurs. Data read from or written to &lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;SRAM before the reset event occurred is retained, and no other address locations are accessed or changed. &lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;In case of no access ongoing when reset occurs, the SRAM corruption does not happen.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Instead, synchronous reset (SW reset) should be used in controlled function (without SRAM accesses) in &lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;case an initialization procedure without SRAM initialization is needed.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you perform functional reset using MC_ME module, content of the RAM will be preserved. If you use destructive reset, you should check the content of the RAM and in case there are some ECC errors for example, you should initialize RAM again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Aug 2017 12:30:44 GMT</pubDate>
    <dc:creator>martin_kovar</dc:creator>
    <dc:date>2017-08-08T12:30:44Z</dc:date>
    <item>
      <title>Problem with Initialize RAM</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Problem-with-Initialize-RAM/m-p/666861#M7526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;I am using MPC5646C with&amp;nbsp;S32 Design Studio for Power v1.2,&lt;BR /&gt;What configuration can make the RAM initialization time without clear operation,&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" data-aligning="#tran_0,#src_0" style="border: 0px;"&gt;Is the means, Mode Control Register (ME_MCTL):&lt;/SPAN&gt;&lt;BR style="color: #434343;" /&gt;&lt;SPAN class="" data-aligning="#tran_1,#src_1" style="border: 0px;"&gt;TARGET_MODE = 0000 RESET (triggers a "functional" RESET event)&amp;nbsp;&lt;BR /&gt;or&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" data-aligning="#tran_1,#src_1" style="border: 0px;"&gt;&lt;SPAN&gt;TARGET_MODE =&amp;nbsp;1111 RESET (triggers a ‘destructive’ reset event)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" data-aligning="#tran_1,#src_1" style="border: 0px;"&gt;&lt;SPAN&gt;Reset after RAM keep reset before the value.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" data-aligning="#tran_1,#src_1" style="border: 0px;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" data-aligning="#tran_1,#src_1" style="border: 0px;"&gt;&lt;SPAN style="background-color: #ffffff; color: #51626f;"&gt;Regards&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" data-aligning="#tran_1,#src_1" style="border: 0px;"&gt;&lt;SPAN style="background-color: #ffffff; color: #51626f;"&gt;Jian&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 06 Aug 2017 05:00:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Problem-with-Initialize-RAM/m-p/666861#M7526</guid>
      <dc:creator>mcmo</dc:creator>
      <dc:date>2017-08-06T05:00:58Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with Initialize RAM</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Problem-with-Initialize-RAM/m-p/666862#M7527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Asynchronous reset will possibly corrupt SRAM if it asserts during a read or write operation to SRAM. &lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;The completion of that access depends on the cycle at which the reset occurs. Data read from or written to &lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;SRAM before the reset event occurred is retained, and no other address locations are accessed or changed. &lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;In case of no access ongoing when reset occurs, the SRAM corruption does not happen.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Instead, synchronous reset (SW reset) should be used in controlled function (without SRAM accesses) in &lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;case an initialization procedure without SRAM initialization is needed.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you perform functional reset using MC_ME module, content of the RAM will be preserved. If you use destructive reset, you should check the content of the RAM and in case there are some ECC errors for example, you should initialize RAM again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Aug 2017 12:30:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Problem-with-Initialize-RAM/m-p/666862#M7527</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2017-08-08T12:30:44Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with Initialize RAM</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Problem-with-Initialize-RAM/m-p/666863#M7528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; font-size: 14px;"&gt;Hello &lt;SPAN&gt;Martin&lt;/SPAN&gt;,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; font-size: 14px;"&gt;&lt;SPAN class="" data-aligning="#tran_0,#src_0" style="color: #666666; background-color: rgba(255, 255, 255, 0.8); border: 0px; font-size: 12px;"&gt;Thank you for your reply, I spent another plan instead of this.&lt;/SPAN&gt;&lt;SPAN class="" data-aligning="#tran_1,#src_1" style="color: #666666; background-color: rgba(255, 255, 255, 0.8); border: 0px; font-size: 12px;"&gt;But I don't know what did the code below to RAM,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; font-size: 14px;"&gt;&lt;SPAN class="" data-aligning="#tran_1,#src_1" style="color: #666666; background-color: rgba(255, 255, 255, 0.8); border: 0px; font-size: 12px;"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;;#***************************** Initialise SRAM ECC ***************************/&lt;BR /&gt;;# Store number of 128Byte (32GPRs) segments in Counter&lt;BR /&gt; e_lis r5, __SRAM_SIZE@h # Initialize r5 to size of SRAM (Bytes)&lt;BR /&gt; e_or2i r5, __SRAM_SIZE@l&lt;BR /&gt; e_srwi r5, r5, 0x7 # Divide SRAM size by 128&lt;BR /&gt; mtctr r5 # Move to counter for use with "bdnz"&lt;/P&gt;&lt;P&gt;;# Base Address of the internal SRAM&lt;BR /&gt; e_lis r5, __SRAM_BASE_ADDR@h&lt;BR /&gt; e_or2i r5, __SRAM_BASE_ADDR@l&lt;/P&gt;&lt;P&gt;;# Fill SRAM with writes of 32GPRs&lt;BR /&gt;sram_loop:&lt;BR /&gt; e_stmw r0,0(r5) # Write all 32 registers to SRAM&lt;BR /&gt; e_addi r5,r5,128 # Increment the RAM pointer to next 128bytes&lt;BR /&gt; e_bdnz sram_loop # Loop for all of SRAM&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; font-size: 14px;"&gt;&lt;SPAN class="" data-aligning="#tran_1,#src_1" style="color: #666666; background-color: rgba(255, 255, 255, 0.8); border: 0px; font-size: 12px;"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; font-size: 14px;"&gt;&lt;SPAN class="" data-aligning="#tran_1,#src_1" style="color: #666666; background-color: rgba(255, 255, 255, 0.8); border: 0px; font-size: 12px;"&gt; the code is in the startup.s file.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In my S32ds debugging, it seems that S32ds will initialize the RAM, I can't confirm whether this code reset the RAM.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;SPAN style="background-color: #ffffff; border: 0px; color: #51626f; font-weight: inherit;"&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;SPAN style="background-color: #ffffff; border: 0px; color: #51626f; font-weight: inherit;"&gt;Jian&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Aug 2017 01:55:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Problem-with-Initialize-RAM/m-p/666863#M7528</guid>
      <dc:creator>mcmo</dc:creator>
      <dc:date>2017-08-09T01:55:09Z</dc:date>
    </item>
  </channel>
</rss>