<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DEVKIT-MPC5478G sample code,FlexCAN receive code does not work, But transmit code works. in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/DEVKIT-MPC5478G-sample-code-FlexCAN-receive-code-does-not-work/m-p/665799#M7466</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Martin,&lt;BR /&gt;Thanks for your support.&lt;BR /&gt;I do connect 120-ohm resistor between CANH and CANL on both sides of the bus.&lt;BR /&gt;But I did not connect&amp;nbsp;the ground pins on both sides.&lt;/DIV&gt;&lt;DIV&gt;In our case, CAN-H/CAN-L lines are&amp;nbsp;connected to the vehicle directly without &amp;nbsp;connecting ground pin.&lt;BR /&gt;I try it according to your suggestions late and back to you.&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Best Regards&lt;/DIV&gt;&lt;DIV&gt;Yuhao Pan&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Jul 2017 02:39:29 GMT</pubDate>
    <dc:creator>yuhaopan</dc:creator>
    <dc:date>2017-07-18T02:39:29Z</dc:date>
    <item>
      <title>DEVKIT-MPC5478G sample code,FlexCAN receive code does not work, But transmit code works.</title>
      <link>https://community.nxp.com/t5/MPC5xxx/DEVKIT-MPC5478G-sample-code-FlexCAN-receive-code-does-not-work/m-p/665795#M7462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;DEVKIT-MPC5478G sample code,FlexCAN receive code does not work, But transmit code works.&lt;/P&gt;&lt;P&gt;I use ValueCAN to connect DEVKIT-MPC5478G with PC , The Sample code flexcan_transmit works good .&lt;/P&gt;&lt;P&gt;see receive.png , The message with ID 0x555 is received by PC..&lt;/P&gt;&lt;P&gt;But the sample code flexcan_receive does not work.&lt;/P&gt;&lt;P&gt;The settings in ValueCAN side is shown in can- baudrate.png.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone meet the the same problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jul 2017 09:05:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/DEVKIT-MPC5478G-sample-code-FlexCAN-receive-code-does-not-work/m-p/665795#M7462</guid>
      <dc:creator>yuhaopan</dc:creator>
      <dc:date>2017-07-12T09:05:22Z</dc:date>
    </item>
    <item>
      <title>Re: DEVKIT-MPC5478G sample code,FlexCAN receive code does not work, But transmit code works.</title>
      <link>https://community.nxp.com/t5/MPC5xxx/DEVKIT-MPC5478G-sample-code-FlexCAN-receive-code-does-not-work/m-p/665796#M7463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ValueCAN3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25303i2983F329FC9A2427/image-size/large?v=v2&amp;amp;px=999" role="button" title="ValueCAN3.png" alt="ValueCAN3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jul 2017 06:03:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/DEVKIT-MPC5478G-sample-code-FlexCAN-receive-code-does-not-work/m-p/665796#M7463</guid>
      <dc:creator>yuhaopan</dc:creator>
      <dc:date>2017-07-14T06:03:11Z</dc:date>
    </item>
    <item>
      <title>Re: DEVKIT-MPC5478G sample code,FlexCAN receive code does not work, But transmit code works.</title>
      <link>https://community.nxp.com/t5/MPC5xxx/DEVKIT-MPC5478G-sample-code-FlexCAN-receive-code-does-not-work/m-p/665797#M7464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I do not know if ValueCAN3 work with MPC5748G FlexCAN interface.&lt;/P&gt;&lt;P&gt;The provider has another product named ValueCAN FD.&lt;/P&gt;&lt;P&gt;It seems for FlexCAN interface, I do not know the difference between ValueCAN3 and ValueCAN FD.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jul 2017 06:08:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/DEVKIT-MPC5478G-sample-code-FlexCAN-receive-code-does-not-work/m-p/665797#M7464</guid>
      <dc:creator>yuhaopan</dc:creator>
      <dc:date>2017-07-14T06:08:14Z</dc:date>
    </item>
    <item>
      <title>Re: DEVKIT-MPC5478G sample code,FlexCAN receive code does not work, But transmit code works.</title>
      <link>https://community.nxp.com/t5/MPC5xxx/DEVKIT-MPC5478G-sample-code-FlexCAN-receive-code-does-not-work/m-p/665798#M7465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have already contacted you via case, so could we please use only one communication channel?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the same answer I have already sent you:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt;"&gt;I tested flexcan_receive example you had sent me in the attachment and it works correct on my side. But I did not use ValueCAN device, because I do not have it, so I had used another microcontroller. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt;"&gt;I changed some parameters little bit (decrease speed to 100kbit/s and changed received ID to 0). &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt;"&gt;From the figure, you sent me I am not sure, if you have correctly terminated CAN bus. Please check, if you have connected 120-ohm resistor between CANH and CANL on both sides of the bus (I see some resistors in the figure, but I am not sure, how are connected and what is the value). I recommend you to connect CAN bus ground pin too. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt;"&gt;To make sure that the ValueCAN device works correct, could you please measure TX signal on the bus and send it to me?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt;"&gt;If you have at least two DEVKIT boards, you can try to load flexcan_transmit project into the first board and flexcan_receive project into the second board and try, if this works correct.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jul 2017 09:15:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/DEVKIT-MPC5478G-sample-code-FlexCAN-receive-code-does-not-work/m-p/665798#M7465</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2017-07-17T09:15:30Z</dc:date>
    </item>
    <item>
      <title>Re: DEVKIT-MPC5478G sample code,FlexCAN receive code does not work, But transmit code works.</title>
      <link>https://community.nxp.com/t5/MPC5xxx/DEVKIT-MPC5478G-sample-code-FlexCAN-receive-code-does-not-work/m-p/665799#M7466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Martin,&lt;BR /&gt;Thanks for your support.&lt;BR /&gt;I do connect 120-ohm resistor between CANH and CANL on both sides of the bus.&lt;BR /&gt;But I did not connect&amp;nbsp;the ground pins on both sides.&lt;/DIV&gt;&lt;DIV&gt;In our case, CAN-H/CAN-L lines are&amp;nbsp;connected to the vehicle directly without &amp;nbsp;connecting ground pin.&lt;BR /&gt;I try it according to your suggestions late and back to you.&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Best Regards&lt;/DIV&gt;&lt;DIV&gt;Yuhao Pan&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jul 2017 02:39:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/DEVKIT-MPC5478G-sample-code-FlexCAN-receive-code-does-not-work/m-p/665799#M7466</guid>
      <dc:creator>yuhaopan</dc:creator>
      <dc:date>2017-07-18T02:39:29Z</dc:date>
    </item>
  </channel>
</rss>