<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: EBI bus interface in MPC5777C controller in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/EBI-bus-interface-in-MPC5777C-controller/m-p/663585#M7366</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the confirmation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Jul 2018 08:02:48 GMT</pubDate>
    <dc:creator>shalakashinde</dc:creator>
    <dc:date>2018-07-23T08:02:48Z</dc:date>
    <item>
      <title>EBI bus interface in MPC5777C controller</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EBI-bus-interface-in-MPC5777C-controller/m-p/663580#M7361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have confusion on how to configure the data and address lines in EBI of MPC5777C controller.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/122628iA0625DD1E24F736D/image-size/large?v=v2&amp;amp;px=999" title="172197_172197.png" alt="172197_172197.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10743i7754FDEC472D543C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I want to use Muxed-32 bit mode (with two 1Mx16 MRAM chips (20 address lines) and two 64Mx16 NOR Flash chips) with chip selects 0 and 1 for MRAM and NOR flash respectively.&lt;/P&gt;&lt;P&gt;As shown in the table above, Address [9:15] are dedicated address pins and functionality will always be address irrespective of mode settings.&lt;/P&gt;&lt;P&gt;D_ADD_DAT[0:15] pins are multiplexed for Add#ress[0:15] and Data[0:15].&lt;/P&gt;&lt;P&gt;First of all, in pin-out of the controller, this name is not mentioned on these pins and it is mentioned as D_DAT[0:15].&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Are these pins really multiplexed? or only function is data?&lt;/P&gt;&lt;P&gt;2. If they are multiplexed with Address[0:15], then Address[9:15] is getting duplicated at two places.&lt;/P&gt;&lt;P&gt;Will it be generated at two set of pins?&lt;/P&gt;&lt;P&gt;3. Address[9:15] can also be configured as GPIOs.&lt;/P&gt;&lt;P&gt;If I do so, will address duplication affect the function of my GPIOs, in case answer to question 2 is yes?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also,&lt;/P&gt;&lt;P&gt;how pins D_OE, D_WE0, D_WE1, D_WE2, D_WE3, D_RD_WR are supposed to be used for different chip selects?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/122629i74DCA96BDCE7A5A6/image-size/large?v=v2&amp;amp;px=999" title="172200_172200.png" alt="172200_172200.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10908i1B2AEC06EC33AE09/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Shalaka&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 06:06:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EBI-bus-interface-in-MPC5777C-controller/m-p/663580#M7361</guid>
      <dc:creator>shalakashinde</dc:creator>
      <dc:date>2016-12-09T06:06:35Z</dc:date>
    </item>
    <item>
      <title>Re: EBI bus interface in MPC5777C controller</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EBI-bus-interface-in-MPC5777C-controller/m-p/663581#M7362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1) Yes, it is marked confused way but these pins can works as D_ADD_DAT[0:15] in multiplexed mode. I will suggest documentation improvement.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) These are duplicated but D_ADD[9:15] contains only address thus they may not be buffered.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;3) Yes, you can use these pins as GPIO if you don’t need it for EBI purpose.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;4) D_OE, D_WE0, D_WE1, D_WE2, D_WE3, D_RD_WR will be shared for all devices connected (if all used, flash memories typically don’t need all WE lines). Only CS lines distinguish between connected device.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 11:48:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EBI-bus-interface-in-MPC5777C-controller/m-p/663581#M7362</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2016-12-09T11:48:10Z</dc:date>
    </item>
    <item>
      <title>Re: EBI bus interface in MPC5777C controller</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EBI-bus-interface-in-MPC5777C-controller/m-p/663582#M7363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;I&lt;/SPAN&gt; &lt;SPAN&gt;already&lt;/SPAN&gt; &lt;SPAN&gt;use&lt;/SPAN&gt; &lt;SPAN&gt;this configuration&lt;/SPAN&gt; &lt;SPAN&gt;with&lt;/SPAN&gt; &lt;SPAN&gt;32-bit bus&lt;/SPAN&gt; &lt;SPAN&gt;and it works.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It&lt;/SPAN&gt; work not on burst mode in my board&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Dec 2016 08:53:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EBI-bus-interface-in-MPC5777C-controller/m-p/663582#M7363</guid>
      <dc:creator>marcellobellini</dc:creator>
      <dc:date>2016-12-12T08:53:06Z</dc:date>
    </item>
    <item>
      <title>Re: EBI bus interface in MPC5777C controller</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EBI-bus-interface-in-MPC5777C-controller/m-p/663583#M7364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks David.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have one more question on this:&lt;/P&gt;&lt;P&gt;In 32-bit muxed mode, will ADD[9:15] be dedicated address lines? Will the address be valid throughout the write or read cycle?&lt;/P&gt;&lt;P&gt;I am basically latching only ADD_DAT[16:31] signals and connecting ADD[9:15] directly to memory to avoid using another latch for ADD_DAT[0:15] signals.&lt;/P&gt;&lt;P&gt;Will this work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Shalaka&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2018 06:43:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EBI-bus-interface-in-MPC5777C-controller/m-p/663583#M7364</guid>
      <dc:creator>shalakashinde</dc:creator>
      <dc:date>2018-07-23T06:43:07Z</dc:date>
    </item>
    <item>
      <title>Re: EBI bus interface in MPC5777C controller</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EBI-bus-interface-in-MPC5777C-controller/m-p/663584#M7365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it is correct.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2018 07:19:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EBI-bus-interface-in-MPC5777C-controller/m-p/663584#M7365</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2018-07-23T07:19:25Z</dc:date>
    </item>
    <item>
      <title>Re: EBI bus interface in MPC5777C controller</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EBI-bus-interface-in-MPC5777C-controller/m-p/663585#M7366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the confirmation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2018 08:02:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EBI-bus-interface-in-MPC5777C-controller/m-p/663585#M7366</guid>
      <dc:creator>shalakashinde</dc:creator>
      <dc:date>2018-07-23T08:02:48Z</dc:date>
    </item>
  </channel>
</rss>