<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5744P with 8MHz Oscillator , Aurora Interface in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-with-8MHz-Oscillator-Aurora-Interface/m-p/662034#M7314</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have tested it only on 40MHz XTAL.&lt;/P&gt;&lt;P&gt;Attached is example of cascaded PLLs.&lt;/P&gt;&lt;P&gt;PLL0 = 160MHz&lt;/P&gt;&lt;P&gt;PLL1 = 200 MHz&lt;/P&gt;&lt;P&gt;But there should be no issue also when you use 8MHz one.&lt;/P&gt;&lt;P&gt;Just follow the RM : 13.5.1.4 PLLDIG initialization information chapter.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: Have in mind that VCO must be in range 600 — 1250 MHz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Nov 2016 12:13:53 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2016-11-21T12:13:53Z</dc:date>
    <item>
      <title>MPC5744P with 8MHz Oscillator , Aurora Interface</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-with-8MHz-Oscillator-Aurora-Interface/m-p/662033#M7313</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have 8MHz Extal instead of 40MHz, for MPC5744P cut2 rev3.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use PLL0 to generate 160MHz (MOTC) and 40MHz (feeding PLL1).&lt;/P&gt;&lt;P&gt;In PLL1 I can generate out of the 40MHz the Sys_clk = 200MHz. This is working, since I can output the 200MHz on the oscilloscope.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But it seems there is some problem with the Aurora interface. I cannot connect to the target with 8MHz and the described settings.&lt;/P&gt;&lt;P&gt;Whereas, when using a 40MHz Xtal which feeds both PLL0 &amp;amp; PLL1 (not the cascaded PLL configuration) I have no problems. (The visualisation tool which establishes the connection to the target is Vector VX1132 and the VX1452 POD for HSSL- high speed serial link via Aurora).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wonder whether I configured everything correctly for the cascaded PLL setting, I also did only find example source using 40MHz Xtal.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;--&amp;gt; !! I also use the xls you provide for clocking, but e.g. there is not the hint like in ref-man:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;NOTE: In cascaded PLL configuration (PLL0 driving the reference clock for PLL1) the external power&lt;BR /&gt;down signal for PLL1 must be removed only when PLL0 has locked, PLL0SR[LOCK] = 1.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;.. do you have example source for cascaded pll ? &amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Lars&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Nov 2016 13:03:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-with-8MHz-Oscillator-Aurora-Interface/m-p/662033#M7313</guid>
      <dc:creator>larskrause</dc:creator>
      <dc:date>2016-11-15T13:03:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P with 8MHz Oscillator , Aurora Interface</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-with-8MHz-Oscillator-Aurora-Interface/m-p/662034#M7314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have tested it only on 40MHz XTAL.&lt;/P&gt;&lt;P&gt;Attached is example of cascaded PLLs.&lt;/P&gt;&lt;P&gt;PLL0 = 160MHz&lt;/P&gt;&lt;P&gt;PLL1 = 200 MHz&lt;/P&gt;&lt;P&gt;But there should be no issue also when you use 8MHz one.&lt;/P&gt;&lt;P&gt;Just follow the RM : 13.5.1.4 PLLDIG initialization information chapter.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: Have in mind that VCO must be in range 600 — 1250 MHz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Nov 2016 12:13:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-with-8MHz-Oscillator-Aurora-Interface/m-p/662034#M7314</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2016-11-21T12:13:53Z</dc:date>
    </item>
  </channel>
</rss>