<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: MPC5744 Datasheet Error About Pin D[12]</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5744-Datasheet-Error-About-Pin-D-12/m-p/661299#M7286</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this reference manual typo is already reported. It should be fixed in addendum, which will be released next month.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Correct function is DSPI3 SOUT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Jan 2017 12:24:01 GMT</pubDate>
    <dc:creator>martin_kovar</dc:creator>
    <dc:date>2017-01-04T12:24:01Z</dc:date>
    <item>
      <title>MPC5744 Datasheet Error About Pin D[12]</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744-Datasheet-Error-About-Pin-D-12/m-p/661298#M7285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is an error in the datasheet of MPC5744P. It is marked with a red box in the attached section of the datasheet.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is not clear which SPI module's (DSPI 1 or DSPI3) SOUT output can be connected to pin D[12].&lt;/P&gt;&lt;P&gt;There are alternative SOUT pins for both of these modules but I hope that&amp;nbsp;this issue leads to an overall check of all SPI module pins.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cagatay&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jan 2017 09:50:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744-Datasheet-Error-About-Pin-D-12/m-p/661298#M7285</guid>
      <dc:creator>cagataykaleliog</dc:creator>
      <dc:date>2017-01-04T09:50:28Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744 Datasheet Error About Pin D[12]</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744-Datasheet-Error-About-Pin-D-12/m-p/661299#M7286</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this reference manual typo is already reported. It should be fixed in addendum, which will be released next month.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Correct function is DSPI3 SOUT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jan 2017 12:24:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744-Datasheet-Error-About-Pin-D-12/m-p/661299#M7286</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2017-01-04T12:24:01Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744 Datasheet Error About Pin D[12]</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744-Datasheet-Error-About-Pin-D-12/m-p/661300#M7287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cagatay&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jan 2017 12:28:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744-Datasheet-Error-About-Pin-D-12/m-p/661300#M7287</guid>
      <dc:creator>cagataykaleliog</dc:creator>
      <dc:date>2017-01-04T12:28:01Z</dc:date>
    </item>
  </channel>
</rss>