<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックQuery on MPC5777C ERM module functionality</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Query-on-MPC5777C-ERM-module-functionality/m-p/659321#M7176</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to test the functionality of MPC5777C EIM(Error Injection Module) and ERM(Error Reporting Module). I have configured to inject errors in the PRAMC_0 and PRAMC_1 channels in the EIM. When I am doing a read access in System RAM at address 0x4000_0000(the memory controlled by PRAMC_0), I would expect that an error be reported in the PRAMC_0 channel in the ERM. However, I am seeing that the error is being reported in the "Core0 data" or "Core1 data" channels(channel numbers: 14,16) in the ERM depending on where my build is loaded and not in the PRAMC_0 channel. On the other hand, when I do a write to the memory, I could see errors being reported in the PRAMC channel in the ERM and nothing reported in "Core data" channels. Could you please explain the reason for this behaviour?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sidhartha.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Feb 2017 06:58:33 GMT</pubDate>
    <dc:creator>sidharthachittu</dc:creator>
    <dc:date>2017-02-22T06:58:33Z</dc:date>
    <item>
      <title>Query on MPC5777C ERM module functionality</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Query-on-MPC5777C-ERM-module-functionality/m-p/659321#M7176</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to test the functionality of MPC5777C EIM(Error Injection Module) and ERM(Error Reporting Module). I have configured to inject errors in the PRAMC_0 and PRAMC_1 channels in the EIM. When I am doing a read access in System RAM at address 0x4000_0000(the memory controlled by PRAMC_0), I would expect that an error be reported in the PRAMC_0 channel in the ERM. However, I am seeing that the error is being reported in the "Core0 data" or "Core1 data" channels(channel numbers: 14,16) in the ERM depending on where my build is loaded and not in the PRAMC_0 channel. On the other hand, when I do a write to the memory, I could see errors being reported in the PRAMC channel in the ERM and nothing reported in "Core data" channels. Could you please explain the reason for this behaviour?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sidhartha.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 06:58:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Query-on-MPC5777C-ERM-module-functionality/m-p/659321#M7176</guid>
      <dc:creator>sidharthachittu</dc:creator>
      <dc:date>2017-02-22T06:58:33Z</dc:date>
    </item>
    <item>
      <title>Re: Query on MPC5777C ERM module functionality</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Query-on-MPC5777C-ERM-module-functionality/m-p/659322#M7177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;EIM injects error to the particular RAM array bus, so it is being detected by the side affected by this error.&lt;/P&gt;&lt;P&gt;If it is write (thus transfer from Core0 to PRAMC_0 with error on the way), it’ll be detected by PRAMC_0.&lt;/P&gt;&lt;P&gt;If it is read (thus transfer from PRAMC_0 to Core0 with error on the way), it’ll be detected by Core0.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you see more errors in more ERM channels at once, if could be possibly caused by enabled cache memory.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 15:53:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Query-on-MPC5777C-ERM-module-functionality/m-p/659322#M7177</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2017-02-22T15:53:53Z</dc:date>
    </item>
  </channel>
</rss>