<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5643L Injection current under non supplied condition</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5643L-Injection-current-under-non-supplied-condition/m-p/659295#M7175</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Peter,&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;Yes, I have already gone through this application note. Do you have any additional information related to my question a) and b).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 May 2017 09:11:34 GMT</pubDate>
    <dc:creator>rakeshshetty</dc:creator>
    <dc:date>2017-05-04T09:11:34Z</dc:date>
    <item>
      <title>MPC5643L Injection current under non supplied condition</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5643L-Injection-current-under-non-supplied-condition/m-p/659293#M7173</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently, in one of our project i am using MPC5643L Leopard Microcontroller. Usually in microcontroller datasheet will specify the value of injection current as 1mA for the supplied condition i.e. VDD=3.0V to 3.6V,considering diode voltage drop of 0.3V. But I have a situation in my application where I am applying signal to the input pin of&amp;nbsp; the microcontroller before the 3.3V supplied, and the time duration is around 50ms ( Input voltage:12V given to voltage divider 51K and 5.11K. PFA) .&lt;/P&gt;&lt;P&gt;I consider this as non-supplied condition, and injection current limit under this condition is not mentioned in datasheet.&lt;/P&gt;&lt;P&gt;I have the following questions which I need some information's.&lt;/P&gt;&lt;P&gt;a) What value of injection current should be considered under this condition? Is there any timelimit?&lt;/P&gt;&lt;P&gt;b) Injection Current is also specified for overload condition i.e 10mA. Whether this overload condition is applicable for transient signals under supplied condition or non supplied condition?&lt;/P&gt;&lt;P&gt;c) Is there any another design consideration, since applying input signals under non supplied condition will result in increase of supply voltage and unintended operation of the MCU has to be prohibited.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.S: This Current configuration can not be avoided in our application&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help is appreciated&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 May 2017 05:47:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5643L-Injection-current-under-non-supplied-condition/m-p/659293#M7173</guid>
      <dc:creator>rakeshshetty</dc:creator>
      <dc:date>2017-05-03T05:47:04Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5643L Injection current under non supplied condition</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5643L-Injection-current-under-non-supplied-condition/m-p/659294#M7174</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;When the power supplies are off, injection current may cause the power supply to rise above 0 volts. In this case, it is&lt;BR /&gt;important to ensure that the voltage is not too large and that the MCU is kept in reset when the voltage is lower than the&lt;BR /&gt;minimum operating voltage of the device.&lt;/P&gt;&lt;P&gt;For more details refer to:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.nxp.com/assets/documents/data/en/application-notes/AN4731.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1" title="http://cache.nxp.com/assets/documents/data/en/application-notes/AN4731.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;http://cache.nxp.com/assets/documents/data/en/application-notes/AN4731.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2017 07:30:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5643L-Injection-current-under-non-supplied-condition/m-p/659294#M7174</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2017-05-04T07:30:30Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5643L Injection current under non supplied condition</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5643L-Injection-current-under-non-supplied-condition/m-p/659295#M7175</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Peter,&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;Yes, I have already gone through this application note. Do you have any additional information related to my question a) and b).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2017 09:11:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5643L-Injection-current-under-non-supplied-condition/m-p/659295#M7175</guid>
      <dc:creator>rakeshshetty</dc:creator>
      <dc:date>2017-05-04T09:11:34Z</dc:date>
    </item>
  </channel>
</rss>