<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Can't I write the UTEST area using Flash driver?</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Can-t-I-write-the-UTEST-area-using-Flash-driver/m-p/658975#M7166</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Experts.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using MPC5777C.&lt;/P&gt;&lt;P&gt;I want to write JTag Password in the UTEST area through flash api which was based on flash driver.&lt;/P&gt;&lt;P&gt;But&amp;nbsp;Verification Fail occurred during writing.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can't I write the UTEST area using Flash driver?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Jaejyn&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Dec 2016 13:41:09 GMT</pubDate>
    <dc:creator>jaejynshin</dc:creator>
    <dc:date>2016-12-08T13:41:09Z</dc:date>
    <item>
      <title>Can't I write the UTEST area using Flash driver?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Can-t-I-write-the-UTEST-area-using-Flash-driver/m-p/658975#M7166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Experts.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using MPC5777C.&lt;/P&gt;&lt;P&gt;I want to write JTag Password in the UTEST area through flash api which was based on flash driver.&lt;/P&gt;&lt;P&gt;But&amp;nbsp;Verification Fail occurred during writing.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can't I write the UTEST area using Flash driver?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Jaejyn&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Dec 2016 13:41:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Can-t-I-write-the-UTEST-area-using-Flash-driver/m-p/658975#M7166</guid>
      <dc:creator>jaejynshin</dc:creator>
      <dc:date>2016-12-08T13:41:09Z</dc:date>
    </item>
    <item>
      <title>Re: Can't I write the UTEST area using Flash driver?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Can-t-I-write-the-UTEST-area-using-Flash-driver/m-p/658976#M7167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The DCF records are not intended to be written via application SW.&lt;/P&gt;&lt;P&gt;User have to write them during development phase. (not in field)&lt;/P&gt;&lt;P&gt;For this purpose use can use debugger (scripts) or via programmer machine in production.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 08:50:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Can-t-I-write-the-UTEST-area-using-Flash-driver/m-p/658976#M7167</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2016-12-15T08:50:08Z</dc:date>
    </item>
  </channel>
</rss>